resources:eval:user-guides:circuits-from-the-lab:cn0364 [14 Jan 2015 09:41]
JB Chua Merged Setup and Connecting Hardware sections
resources:eval:user-guides:circuits-from-the-lab:cn0364 [06 Jan 2021 08:28] (current)
Ioana Chelaru Fixed bad link for EVAL-CN0364-SDPZ and removed reference for EVAL-SDP-CB1Z
Line 6: Line 6:
 The [[ADI>​ADuM5211]] and [[ADI>​ADuM3151]] provide digital line and power isolation. The [[ADI>​ADP2441]] 36 V, step-down, dc-to-dc regulator accepts an industrial standard 24 V supply, with wide tolerance on the input voltage and steps it down to 5V to be used by the system. ​       ​ The [[ADI>​ADuM5211]] and [[ADI>​ADuM3151]] provide digital line and power isolation. The [[ADI>​ADP2441]] 36 V, step-down, dc-to-dc regulator accepts an industrial standard 24 V supply, with wide tolerance on the input voltage and steps it down to 5V to be used by the system. ​       ​
  
-This user guide will discuss how to use the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and evaluation software to configure and collect data from the EVAL-CN0364-SDPZ Evaluation Board **(CN-0364 Board)**. The evaluation board also has PMOD compatible headers for connection to other processors or microcontrollers.+This user guide will discuss how to use the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and evaluation software to configure and collect data from the EVAL-CN0364-SDPZ Evaluation Board **(CN-0364 Board)**. The evaluation board also has PMOD compatible headers for connection to other processors or microcontrollers.
  
-A complete design support package for the [[adi>​EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[http://​www.analog.com/​CN0364-Shield-DesignSupport|CN0364-Shield-DesignSupport]].+A complete design support package for the [[adi>CN0364|EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0364-DesignSupport|CN0364-DesignSupport]].
  
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​cn0364.jpg?​nolink&​300 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​cn0364.jpg?​nolink&​300 |}}
Line 15: Line 15:
  
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ Evaluation Board]] +  * [[adi>​CN0364|EVAL-CN0364-SDPZ Evaluation Board]] 
-  * [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] ​Controller Board (**SDP-B Board**)+  * EVAL-SDP-CB1Z Controller Board (**SDP-B Board**)
   * DC Power Supply (+12V to +24V)   * DC Power Supply (+12V to +24V)
   * Precision voltage and current source (for input)   * Precision voltage and current source (for input)
-  * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0364/​|CN0364Evaluation ​Software]]+  * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0364/​|CN0364 Evaluation ​Software]]
   * PC with the following //Minimum Requirements//​   * PC with the following //Minimum Requirements//​
       * Windows Vista/7 (32-bit)       * Windows Vista/7 (32-bit)
Line 31: Line 31:
 ===== General Setup ===== ===== General Setup =====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​setup-1.png?​nolink&​300 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​setup-1.png?​nolink&​300 |}}
-  * The [[http://​www.analog.com/​EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector +  * The [[adi>CN0364|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector 
-  * The [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.+  * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
   * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC   * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC
   * Header **P11** is a PMOD compatible UART header - allows for communication to the HART modem   * Header **P11** is a PMOD compatible UART header - allows for communication to the HART modem
Line 38: Line 38:
   * Terminal blocks **P1**,​**P2**,​**P3** and **P4** provide the quad channel voltage input (-10V to +10V)   * Terminal blocks **P1**,​**P2**,​**P3** and **P4** provide the quad channel voltage input (-10V to +10V)
   * Terminal blocks **P5**,​**P6**,​**P7** and **P8** provide the quad channel HART-compatible,​ 4 mA to 20 mA current inputs   * Terminal blocks **P5**,​**P6**,​**P7** and **P8** provide the quad channel HART-compatible,​ 4 mA to 20 mA current inputs
 +
 +See image for terminal block assignments:​
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​board_connections.png?​nolink&​600 |}}
  
 **Jumper Settings** **Jumper Settings**
Line 114: Line 117:
     * Display for the address variables received from the HART-enabled device via CMD 0     * Display for the address variables received from the HART-enabled device via CMD 0
   - **Device Variables**  ​   - **Device Variables**  ​
-    * Display for the device variables received from the HART-enabled device via CMD 0+    * Display for the device variables received from the HART-enabled device via CMD 3
   - **Device Status**  ​   - **Device Status**  ​
     * Display for the reported status information from the HART enabled device     * Display for the reported status information from the HART enabled device
Line 160: Line 163:
   - Click the **OK Button**.   - Click the **OK Button**.
 <WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</​WRAP>​ <WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</​WRAP>​
 +
 +----
 +
 +===== More Information and Useful Links =====
 +  * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0364/​|CN0364 Evaluation Software]]
 +  * [[ADI>​CN0364|CN0364 Circuit Note Page]]
 +  * [[ADI>​CN0364-DesignSupport|CN0364 Design Support Package]]
 +  * [[ADI>​AD7173-8|AD7173-8 Product Page]]
 +  * [[ADI>​AD5700-1|AD5700-1 Product Page]]
 +  * [[ADI>​ADUM5211|ADUM5211 Product Page]]
 +  * [[ADI>​ADUM3151|ADUM3151 Product Page]]
 +  * [[ADI>​ADP2441|ADP2441Product Page]]
 +  * [[ADI>​ADG704|ADG704Product Page]]
resources/eval/user-guides/circuits-from-the-lab/cn0364.1421224899.txt.gz · Last modified: 14 Jan 2015 09:41 by JB Chua