This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guides:circuits-from-the-lab:cn0359 [29 Jul 2021 09:13] – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== CN0359 Conductivity Measurement System User Guide ====== | ||
+ | ===== Overview ===== | ||
+ | |||
+ | Completely self-contained, | ||
+ | |||
+ | A carefully selected combination of precision signal conditioning components yields an accuracy of better than 0.3% over a conductivity range of 0.1 μS to 10 S (10 MΩ to 0.1 Ω) with no calibration requirements. | ||
+ | |||
+ | Automatic detection is provided for either 100 Ω or 1000 Ω platinum (Pt) resistance temperature devices (RTDs), allowing the conductivity measurement to be referenced to 25°C. | ||
+ | |||
+ | The system accommodates 2- or 4-wire conductivity cells, and 2-, 3-, or 4-wire RTDs for added accuracy and flexibility. | ||
+ | |||
+ | ====== Hardware Connections ====== | ||
+ | |||
+ | The following sections will describe the hardware in more detail. | ||
+ | |||
+ | The CN0359 have 5 connectors: | ||
+ | * **J1** for power supply | ||
+ | * **J2** for RS-485 communication | ||
+ | * **J3** for RTD temperature sensor | ||
+ | * **J4** for JTAG/SWD debug | ||
+ | * **J5** for conductivity sensor | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | To evaluate the full function of CN0359, you need following equipment: | ||
+ | * EVAL-CN0359-EB1Z evaluation board | ||
+ | * EVAL-CFTL-6V-PWRZ 6V DC wall connector | ||
+ | * 2-wire and 4-wire conductivity cells | ||
+ | * 2-wire and 3-wire and 4-wire PT100 and PT1000 RTDs | ||
+ | * A PC with Microsoft Windows 7 or later OS and USB 2.0 or faster USB port | ||
+ | * A USB to RS-485 convert cable | ||
+ | |||
+ | To reprogram or debug CN0359, you need following extra equipment | ||
+ | * J-link debug cable or equivalent JTAG/SWD debug cable | ||
+ | |||
+ | ===== RTD Connections ===== | ||
+ | |||
+ | The CN0359 can support PT100 and PT1000 type of RTD sensors connected in 2-wire or 3-wire or 4-wire mode. The RTD type and connection mode is automatically detect by software. The RTD temperature sensor on the EVAL-CN0359-EB1Z should be connected to header **J3**. | ||
+ | |||
+ | The J3 pin map is following: | ||
+ | | Pin Number | Signal Name | Pin Description | | ||
+ | | Pin 1 | I(+) | Source Excitation Current | | ||
+ | | Pin 2 | V(+) | High Voltage Potential Output | | ||
+ | | Pin 3 | V(-) | Low Voltage Potential Output | | ||
+ | | Pin 4 | I(-) | Sink Excitation Current | | ||
+ | |||
+ | The I signal inject the constant excitation current into RTD, the V signal output will be sample by ADC to measure, the connections for different wire mode please reference following picture. | ||
+ | |||
+ | **RTD 4-wire connection** | ||
+ | {{ : | ||
+ | ---- | ||
+ | |||
+ | **RTD 3-wire connection** | ||
+ | {{ : | ||
+ | |||
+ | ---- | ||
+ | |||
+ | **RTD 2-wire connection** | ||
+ | {{ : | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Conductivity Sensor Connections ===== | ||
+ | |||
+ | The CN0359 support both 2-electrode and 4-electrode conductivity sensor. The conductivity sensor connect to **J5** of the EVAL-CN0359-EB1Z. | ||
+ | |||
+ | The J5 pin map is following: | ||
+ | | Pin Number | Signal Name | Pin Description | | ||
+ | | Pin 1 | I(+) | Source Excitation Current | | ||
+ | | Pin 2 | V(+) | High Voltage Potential Output | | ||
+ | | Pin 3 | V(-) | Low Voltage Potential Output | | ||
+ | | Pin 4 | I(-) | Sink Excitation Current | | ||
+ | | Pin 5 | GND | Ground | | ||
+ | |||
+ | <note tip> | ||
+ | The EVAL-CN0359-EB1Z board error specification is +/- 0.3% under conductivity range: 0.1 μS to 10 S (10 MΩ to 0.1 Ω) condition, if the conductivity range you are using is out of specification, | ||
+ | </ | ||
+ | |||
+ | The connections for different sensor please reference following picture: | ||
+ | |||
+ | **2-electrode conductivity sensor connection** | ||
+ | {{ : | ||
+ | |||
+ | <note important> | ||
+ | If using 2-electrode sensors connected to CN0359 | ||
+ | * pin1 ⇔ pin2 of J5 **MUST** be shorted | ||
+ | * pin3 ⇔ pin4 of J5 **MUST** be shorted | ||
+ | </ | ||
+ | |||
+ | ---- | ||
+ | |||
+ | **4-electrode conductivity sensor connection** | ||
+ | {{ : | ||
+ | |||
+ | ---- | ||
+ | |||
+ | The I signal inject the excitation current into conductivity sensor, after the amplifier the I and V signal will be sample by ADC to measure. | ||
+ | |||
+ | ===== RS-485 interface connections ===== | ||
+ | |||
+ | The EVAL-CN0359-EB1Z **J2** is RS-485 connector. | ||
+ | |||
+ | The J2 pin map is following: | ||
+ | | Pin Number | Signal Name | Pin Description | | ||
+ | | Pin 1 | B | RS-485 B Signal | | ||
+ | | Pin 2 | GND | Ground | | ||
+ | | Pin 3 | A | RS-485 A Signal | | ||
+ | |||
+ | <note tip>The CN0359 software support up to 254 (RS-485 address from 1 to 254) boards connected to one RS-485 network, but for the noise performance the RS-485 terminal resistor R10 on EVAL-CN0359-EB1Z PCB is set to 10kΩ, if you want to use multiply devices on same RS-485 network maybe you need to change or remove R10 to following the RS-485 standard, for more detail about RS-485 network please reference www.analog.com/ | ||
+ | |||
+ | **RS-485 pin map** | ||
+ | {{ : | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== JTAG/SWD connections ===== | ||
+ | |||
+ | The EVAL-CN0359-EB1Z **J4** is the JTAG/SWD debug connector. | ||
+ | |||
+ | The EVAL-CN0359-EB1Z JTAG/SWD debug interface only support SWD debug mode. | ||
+ | |||
+ | ====== Usage Instructions ====== | ||
+ | |||
+ | The CN0359 system runs using a 6V DC wall connector (EVAL-CFTL-6V-PWRZ) and will run automatically when the power on. The system has two interfaces to show the conductivity and RTD results: LCD screen and RS-485 interface, and those two interfaces can working simultaneously as well. | ||
+ | |||
+ | <note tip>The CN0359 usage is depend on the software version, maybe there have difference between following instructions and shipped CN0359, please check [[adi> | ||
+ | |||
+ | The CN0359 has the following opinions which can be set by the user: | ||
+ | * Excitation voltage | ||
+ | * Excitation frequency | ||
+ | * Track-hold setup time | ||
+ | * Track-hold hold time | ||
+ | * Temperature coefficient | ||
+ | * Conductivity cell constant | ||
+ | * RS-485 baud rate | ||
+ | * RS-485 address | ||
+ | * LCD contrast | ||
+ | |||
+ | <note warning> | ||
+ | |||
+ | ===== LCD Screen and Encoder User Interface ===== | ||
+ | |||
+ | The LCD screen can show the measurement results and settings of CN0359, user interactive with CN0359 could be done using the LCD and encoder **S1**. | ||
+ | |||
+ | ==== General usage instructions ==== | ||
+ | |||
+ | The CN0359 LCD display area have 3 status with different meaning: | ||
+ | * normal status (dark font with light background) ⇒ item normal displayed | ||
+ | * reverse status (light font with dark background) ⇒ item has been selected | ||
+ | * blink status (keep flipping between normal status and reverse status) → item has been selected and in value chang status | ||
+ | |||
+ | The CN0359 encoder **S1** can be turned clockwise or counterclockwise (no mechanical stop), and can also be used as a push button. The following is the encoder operating meaning: | ||
+ | * turn clockwise at reverse status ⇒ change selection to next item. | ||
+ | * turn clockwise at blink status ⇒ increase value | ||
+ | * turn counterclockwise at reverse status ⇒ change selection to previous item | ||
+ | * turn counterclockwise at blink status ⇒ decrease value | ||
+ | * push button at reverse status ⇒ enter selected item | ||
+ | * push button at blink status ⇒ exit blinked item | ||
+ | |||
+ | < | ||
+ | There have two exception dialogs: | ||
+ | * home dialog ⇒ no selected item in this dialog, push button will enter setting menu | ||
+ | * LCD contrast setting dialog ⇒ in case the LCD display abnormal there is no blinked item in this dialog, turn encoder clockwise/ | ||
+ | </ | ||
+ | |||
+ | The CN0359 have a buzzer on PCB, it will beeping when value limit reached or notify asserted. | ||
+ | |||
+ | ==== CN0359 start up and LCD contrast ==== | ||
+ | |||
+ | The CN0359 LCD screen contrast can be set by user, if the LCD contrast value set improper it will cause LCD display murky dull or have crosstalk, in this case user need to recover LCD contrast blindly, the following step can adjust LCD contrast blindly: | ||
+ | - power up CN0359, the CN0359 will beep for 50ms immediately, | ||
+ | - the LCD should be showing the splash screen for 3s, maybe LCD show nothing or black screen if the contrast set improper, please push encoder button **S1** within 3s from powering on in splash screen. | ||
+ | - the CN0359 will beeping 100ms two times, interval 100ms, this means the CN0359 entered LCD contrast setting status | ||
+ | - turning the encoder **S1** clockwise/ | ||
+ | - push button **S1** return to setting dialog | ||
+ | - enter "reurn to home" menu item, CN0359 LCD will display properly and contrast setting will be saved | ||
+ | |||
+ | ==== Buzzer and Alarm ==== | ||
+ | The EVAL-CN0359-EB1Z board have a buzzer **U2** on it, the buzzer will beeping in the following cases: | ||
+ | * notify beeping 50ms at power up | ||
+ | * notify beeping 200ms when from splash screen entering home dialog | ||
+ | * notify beeping 100ms twice, interval 100ms, when button pushed at splash screen, entering LCD contrast setting dialog | ||
+ | * alarm beeping 50ms for 5 times, interval 50ms when startup internal error, then means all the settings restore to default value, if this error asserted, please set all the settings to requirement | ||
+ | * alarm beeping 10ms at home dialog when RTD error, if this error asserted, please check RTD connection | ||
+ | * alarm beeping 100ms at home dialog when conductivity sensor error, if this error asserted, please check conductivity sensor connection | ||
+ | * notify beeping 10ms if encoder turned to against software limit | ||
+ | |||
+ | |||
+ | |||
+ | ===== RS-485 Interface ===== | ||
+ | |||
+ | The RS-485 interface can connect multi (up to 254) CN0359 in the same RS-485 network, in the following chapter the CN0359 in the RS-485 network will be called client, the PC or any type of RS-485 device who can initiate the communications will be called host. Please notice: because the CN0359 use the single duplex mode RS-485 network, so there only one device can send the data at the same time, otherwise the RS-485 network will involve into the signal conflict, this will cause unpredictable result. In usually the CN0359 RS-485 network have only one host, if you have multi host in the network, please make sure there is no conflict occur in any time. | ||
+ | |||
+ | The in the RS-485 network all the clients will keep in receive status in idle time. The client only send data when it response the right command. | ||
+ | |||
+ | <note important 80%> | ||
+ | The EVAL-CN0359-EB1Z board RS-485 address can only be set by LCD interface. | ||
+ | </ | ||
+ | ==== RS-485 command usage ==== | ||
+ | |||
+ | <note tip>In order to use the RS-485 interface, a terminal program such as [[http:// | ||
+ | |||
+ | The CN0359 command format is following: | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **address** **command** [options] | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | **address** is the integer value of CN0359 address, range from 1 to 254, the **address** should be issue before any command to wake corresponding CN0359 to receive **command** | ||
+ | |||
+ | <note tip> | ||
+ | The CN0359 RS-485 interface use char ' | ||
+ | |||
+ | The CN0359 use char ' ' space character as delimiter, please make sure no ' ' space character lost in command string. | ||
+ | </ | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === poll === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | poll - query setting and result | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **poll** | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **poll** command use to query the CN0359 for setting measurement result. | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 poll | ||
+ | |||
+ | will query the address 100 of CN0359 for setting and result | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === setvolt === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | setvolt - set excitation voltage | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **setvolt** __voltage__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **setvolt** command use to set the excitation voltage, the __voltage__ is peak value of voltage, __voltage__ is float type number range from 0.1 to 10 | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 setvolt 2.5 | ||
+ | |||
+ | will set the address 100 of CN0359 excitation voltage to 2.5V | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === setfreq === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | setfreq - set excitation frequency | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **setfreq** __frequency__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **setfreq** command use to set the excitation frequency, __frequency__ is float type number range from 10 to 100000 | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 setfreq 85.6 | ||
+ | |||
+ | will set the address 100 of CN0359 excitation frequency to 85.6Hz | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === setk === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | setk - set cell constant | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **setk** __K__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **setk** command use to set the cell constant, __K__ is float type number range from 0.01 to 100 | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 setk 1.268 | ||
+ | |||
+ | will set the address 100 of CN0359 cell constant to 1.268/cm | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === setcof === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | setcof - set temperature coefficient | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **setcof** __coefficient__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **setcof** command use to set the temperature coefficient, | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 setcof -2.58 | ||
+ | |||
+ | will set the address 100 of CN0359 temperature coefficient to -2.58%/°C | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === setstm === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | setstm - set track-hold setup time | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **setstm** __time__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **setstm** command use to set the track-hold setup time, the __time__ is the percentage of half excitation period, __time__ is float type number range from 0 to 80 | ||
+ | |||
+ | < | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 setcof 5.8 | ||
+ | |||
+ | will set the address 100 of CN0359 track-hold setup time to 5.8% of half excitation period. If excitation frequency is 100Hz, the half of excitation period will be 5ms, track-hold setup time will be 290us | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === sethtm === | ||
+ | |||
+ | **NAME** | ||
+ | |||
+ | sethtm - set track-hold hold time | ||
+ | |||
+ | **SYNOPSIS** | ||
+ | |||
+ | **sethtm** __time__ | ||
+ | |||
+ | **DESCRIPTION** | ||
+ | |||
+ | The **sethtm** command use to set the track-hold hold time, the __time__ is the percentage of half excitation period, __time__ is float type number range from 0 to 10 | ||
+ | |||
+ | < | ||
+ | |||
+ | This example: | ||
+ | |||
+ | 100 sethtm 1.5 | ||
+ | |||
+ | will set the address 100 of CN0359 track-hold hold time to 1.5% of half excitation period. If excitation frequency is 1kHz, the half of excitation period will be 500us, track-hold hold time will be 7.5us | ||
+ | |||
+ | ====== Software Programming ====== | ||
+ | |||
+ | In this section we are going to talk about how to program the EVAL-CN0359-EB1Z. | ||
+ | |||
+ | ===== How to download binary firmware to the CN0359 ===== | ||
+ | |||
+ | The EVAL-CN0359-EB1Z evaluation board have a JTAG/SWD debug interface **J4**, the **J4** connector is 0.1 inch pitch 20 pins male header, the header pin map compatible with [[https:// | ||
+ | |||
+ | The following step will download the binary firmware to EVAL-CN0359-EB1Z evaluation board: | ||
+ | |||
+ | - Download latest [[https:// | ||
+ | - Download latest [[adi> | ||
+ | - Install J-Link Software and Documentation Pack to your computer following the instructions in package | ||
+ | - Extract //CN0359 Design & Integration Files// to your computer hard disk | ||
+ | - Extract //CN0359 source code package// in //CN0359 Design & Integration Files// to your computer hard disk | ||
+ | - Find the " | ||
+ | - Connect J-Link debug probe to the USB port of your computer and EVAL-CN0359-EB1Z evaluation board **J4** | ||
+ | - Power on EVAL-CN0359-EB1Z evaluation board | ||
+ | - Open J-Link from command line < | ||
+ | SEGGER J-Link Commander V6.00i (Compiled Sep 2 2016 19:25:27) | ||
+ | DLL version V6.00i, compiled Sep 2 2016 19:25:12 | ||
+ | Connecting to J-Link via USB...O.K. | ||
+ | Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46 | ||
+ | Hardware version: V8.00 | ||
+ | S/N: | ||
+ | License(s): RDI, | ||
+ | VTref = 3.300V | ||
+ | Type " | ||
+ | - In J-Link command line terminal input command: //**device ADuCM360**// | ||
+ | J-Link> | ||
+ | - In J-Link command line terminal input command: //**if swd**// press return < | ||
+ | J-Link> | ||
+ | Selecting SWD as current target interface. </ | ||
+ | - In J-Link command line terminal input command: //**speed 4000**// press return < | ||
+ | J-Link> | ||
+ | Selecting 4000 kHz as target interface speed </ | ||
+ | - In J-Link command line terminal input command: // | ||
+ | J-Link> | ||
+ | Target connection not established yet but required for command. | ||
+ | Device " | ||
+ | Found SWD-DP with ID 0x2BA01477 | ||
+ | AP-IDR: 0x24770011, Type: AHB-AP | ||
+ | Found Cortex-M3 r2p0, Little endian. | ||
+ | FPUnit: 6 code (BP) slots and 2 literal slots | ||
+ | CoreSight components: | ||
+ | ROMTbl 0 @ E00FF000 | ||
+ | ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 002BB000 SCS | ||
+ | ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 002BB002 DWT | ||
+ | ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB | ||
+ | Cortex-M3 identified. | ||
+ | Erasing device (ADUCM360)... | ||
+ | Comparing flash | ||
+ | Erasing flash | ||
+ | Verifying flash | ||
+ | J-Link: Flash download: Total time needed: 5.630s (Prepare: 0.063s, Compare: 0.000s, Erase: 5.564s, Program: 0.000s, Verify: 0.000s, Restore: 0.003s) | ||
+ | Erasing done. </ | ||
+ | - In J-Link command line terminal input command: // | ||
+ | J-Link> | ||
+ | Downloading file [x: | ||
+ | Comparing flash | ||
+ | Erasing flash | ||
+ | Programming flash [100%] Done. | ||
+ | Verifying flash | ||
+ | J-Link: Flash download: Flash programming performed for 1 range (76288 bytes) | ||
+ | J-Link: Flash download: Total time needed: 5.945s (Prepare: 0.065s, Compare: 0.529s, Erase: 0.023s, Program: 5.157s, Verify: 0.131s, Restore: 0.038s) | ||
+ | O.K. </ | ||
+ | - After downloading the program, remove J-Link debug probe and power off EVAL-CN0359-EB1Z evaluation board | ||
+ | - Upon next power on, the EVAL-CN0359-EB1Z evaluation board will run new downloaded program | ||
+ | |||
+ | <note tip>the J-Link debug probe detailed usage instructions can be found at [[https:// | ||
+ | ===== Software development environment ===== | ||
+ | |||
+ | The CN0359 software source code could be download at: [[adi> | ||
+ | |||
+ | The tools for CN0359 development could be downloaded at following list: | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[http:// | ||
+ | |||
+ | Please refer to the handbook of each tools for detail usage instructions. | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | ===== Software Structure ===== | ||
+ | |||
+ | The CN0359 software divided in to 3 layers, from top to bottom is: | ||
+ | * application layer | ||
+ | * newlib | ||
+ | * hardware abstraction layer | ||
+ | |||
+ | All the devices is abstracted to the file, the application read and write device file to communicate with hardware. | ||
+ | |||
+ | The following chart is the source file structure: | ||
+ | |||
+ | ├── applications | ||
+ | │ ├── command | ||
+ | │ │ ├── cmd_cellconstant.cpp | ||
+ | │ │ ├── cmd_coefficient.cpp | ||
+ | │ │ ├── cmd_frequency.cpp | ||
+ | │ │ ├── cmd_holdtime.cpp | ||
+ | │ │ ├── cmd_poll.cpp | ||
+ | │ │ ├── cmd_setuptime.cpp | ||
+ | │ │ └── cmd_voltage.cpp | ||
+ | │ ├── dialog | ||
+ | │ │ ├── AddressDialog.cpp | ||
+ | │ │ ├── BaudRateDialog.cpp | ||
+ | │ │ ├── CellConstantDialog.cpp | ||
+ | │ │ ├── CoefficientDialog.cpp | ||
+ | │ │ ├── ContrastDialog.cpp | ||
+ | │ │ ├── Dialog.cpp | ||
+ | │ │ ├── FirmwareDialog.cpp | ||
+ | │ │ ├── FrequencyDialog.cpp | ||
+ | │ │ ├── HoldTimeDialog.cpp | ||
+ | │ │ ├── HomeDialog.cpp | ||
+ | │ │ ├── SettingDialog.cpp | ||
+ | │ │ ├── SetupTimeDialog.cpp | ||
+ | │ │ ├── SplashDialog.cpp | ||
+ | │ │ └── VoltageDialog.cpp | ||
+ | │ ├── main.cpp | ||
+ | │ ├── message.cpp | ||
+ | │ └── uart_exec.cpp | ||
+ | ├── hal | ||
+ | │ ├── devices.cpp | ||
+ | │ ├── drivers | ||
+ | │ │ ├── ad8253.cpp | ||
+ | │ │ ├── adc.cpp | ||
+ | │ │ ├── buzzer.cpp | ||
+ | │ │ ├── dac.cpp | ||
+ | │ │ ├── dma.cpp | ||
+ | │ │ ├── encoder.cpp | ||
+ | │ │ ├── flash.cpp | ||
+ | │ │ ├── lcd.cpp | ||
+ | │ │ ├── pwm.cpp | ||
+ | │ │ └── uart.cpp | ||
+ | │ ├── Exceptions.cpp | ||
+ | │ ├── RTD.cpp | ||
+ | │ ├── syscalls.cpp | ||
+ | │ └── timer.cpp | ||
+ | ├── include | ||
+ | │ ├── applications | ||
+ | │ │ ├── command | ||
+ | │ │ │ ├── cmd_cellconstant.h | ||
+ | │ │ │ ├── cmd_coefficient.h | ||
+ | │ │ │ ├── cmd_frequency.h | ||
+ | │ │ │ ├── cmd_holdtime.h | ||
+ | │ │ │ ├── cmd_poll.h | ||
+ | │ │ │ ├── cmd_setuptime.h | ||
+ | │ │ │ └── cmd_voltage.h | ||
+ | │ │ ├── dialog | ||
+ | │ │ │ ├── AddressDialog.h | ||
+ | │ │ │ ├── BaudRateDialog.h | ||
+ | │ │ │ ├── CellConstantDialog.h | ||
+ | │ │ │ ├── CoefficientDialog.h | ||
+ | │ │ │ ├── ContrastDialog.h | ||
+ | │ │ │ ├── Dialog.h | ||
+ | │ │ │ ├── FirmwareDialog.h | ||
+ | │ │ │ ├── FrequencyDialog.h | ||
+ | │ │ │ ├── HoldTimeDialog.h | ||
+ | │ │ │ ├── HomeDialog.h | ||
+ | │ │ │ ├── SettingDialog.h | ||
+ | │ │ │ ├── SetupTimeDialog.h | ||
+ | │ │ │ ├── SplashDialog.h | ||
+ | │ │ │ └── VoltageDialog.h | ||
+ | │ │ ├── message.h | ||
+ | │ │ └── uart_exec.h | ||
+ | │ └── hal | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | │ | ||
+ | └── system | ||
+ | ├── cmsis | ||
+ | │ ├── startup_ADuCM360.S | ||
+ | │ └── system_ADuCM360.c | ||
+ | └── include | ||
+ | └── cmsis | ||
+ | ├── ADuCM360.h | ||
+ | ├── arm_common_tables.h | ||
+ | ├── arm_const_structs.h | ||
+ | ├── arm_math.h | ||
+ | ├── cmsis_armcc.h | ||
+ | ├── cmsis_armcc_V6.h | ||
+ | ├── cmsis_device.h | ||
+ | ├── cmsis_gcc.h | ||
+ | ├── core_cm0.h | ||
+ | ├── core_cm0plus.h | ||
+ | ├── core_cm3.h | ||
+ | ├── core_cm4.h | ||
+ | ├── core_cm7.h | ||
+ | ├── core_cmFunc.h | ||
+ | ├── core_cmInstr.h | ||
+ | ├── core_cmSimd.h | ||
+ | ├── core_sc000.h | ||
+ | ├── core_sc300.h | ||
+ | └── system_ADuCM360.h | ||
+ | |||
+ | * the **applications** folder contained all application layer source, it include all RS-485 command and LCD dialog routines. | ||
+ | * the **hal** folder contained all hardware abstraction layer source, each of device has his own driver file in this folder to access newlib low level interface. | ||
+ | * the **include** and **system** folder is ADuCM360 support file for external declaration and cortex-m3 cmsis library support. | ||
+ | |||
+ | ====== Schematic, Bill of Materials, Gerber Files, Source Code ====== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | EVAL-CN0359-EB1Z Rev A Files | ||
+ | * {{: | ||
+ | * {{: | ||
+ | * {{: | ||
+ | * {{: | ||
+ | |||
+ | EVAL-CN0359-EB1Z Rev 0 Files | ||
+ | * {{: | ||
+ | * {{: | ||
+ | * {{: | ||
+ | * {{: | ||
+ | </ | ||
+ | |||
+ | ====== Change Log ====== | ||
+ | |||
+ | Rev0 to RevA: | ||
+ | * U1 (from MCCOG128064A6S-SPTLY to BTHQ128064AVC1-COG-STF-LED) | ||
+ | * U7 (from ADM3483ARZ to ADM3075EARZ) | ||
+ | * C32 (from 330n to NP) | ||
+ | * Software (conductivity result reliability routines removed) | ||
+ | * Software (setup and hold time setting added) | ||
+ | * Software (RS-485 communication routines added) | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |