Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0357 [29 Jul 2021 07:48]
Harvey John De Chavez Hardware Registration
resources:eval:user-guides:circuits-from-the-lab:cn0357 [15 Aug 2022 03:59]
Allan Uy
Line 17: Line 17:
   * [[adi>​SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Interposer Board (**SDP to Pmod Interposer Board**)   * [[adi>​SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Interposer Board (**SDP to Pmod Interposer Board**)
   * [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent   * [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent
-  * [[ftp://ftp.analog.com/​pub/​cftl/​CN0357/​|CN0357 Evaluation Software]] +  * [[https://swdownloads.analog.com/​cse/​cftl/​CN0357/​1.0.0/​CN0357_Evaluation_Software.zip|CN0357 Evaluation Software]]
-    * (supplied with provided CD in kit)+
   * PC with the following //Minimum Requirements//​   * PC with the following //Minimum Requirements//​
     * Windows XP Service Pack 2 (32-bit)     * Windows XP Service Pack 2 (32-bit)
Line 33: Line 32:
 ---- ----
 ===== Installing the Software ===== ===== Installing the Software =====
-  - Extract the file **CN0357_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>​**NOTE:​** It is recommended that you install the [[ftp://ftp.analog.com/​pub/​cftl/​CN0357/​|CN-0357 ​Evaluation Software]] to the default directory path **C:​\Program Files\Analog Devices\CN0357\** and all National Instruments products to **C:​\Program Files\National Instruments\**</​WRAP>​\\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install1.png?​nolink&​|}}+  - Extract the file **CN0357_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>​**NOTE:​** It is recommended that you install the [[https://swdownloads.analog.com/​cse/​cftl/​CN0357/​1.0.0/​CN0357_Evaluation_Software.zip|CN0357 ​Evaluation Software]] to the default directory path **C:​\Program Files\Analog Devices\CN0357\** and all National Instruments products to **C:​\Program Files\National Instruments\**</​WRAP>​\\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install1.png?​nolink&​|}}
   - Click **Next** to view the installation review page\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install2.png?​nolink&​|}}\\ \\    - Click **Next** to view the installation review page\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install2.png?​nolink&​|}}\\ \\ 
   - Click **Next** to start the installation\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install3.png?​nolink&​|}}\\ \\    - Click **Next** to start the installation\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0357:​cn0357-install3.png?​nolink&​|}}\\ \\ 
resources/eval/user-guides/circuits-from-the-lab/cn0357.txt · Last modified: 15 Aug 2022 03:59 by Allan Uy