Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0354 [06 Jan 2021 08:30] – Fixed bad link for EVAL-CN0354-PMDZ Ioana Chelaru | resources:eval:user-guides:circuits-from-the-lab:cn0354 [25 Jan 2021 11:09] – Fixed bad link for SDP-I-PMOD Ioana Chelaru |
---|
===== Required Equipment ===== | ===== Required Equipment ===== |
* [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[adi>en/evaluation/eval_sdp-pmod/eb.html|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) | * [[adi>eval_sdp-pmod|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) |
* [[adi>CN0354|EVAL-CN0354-PMDZ]] Evaluation Board (**CN-0354 Board**) | * [[adi>CN0354|EVAL-CN0354-PMDZ]] Evaluation Board (**CN-0354 Board**) |
* [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] +6V Power Supply or equivalent DC Power Supply | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] +6V Power Supply or equivalent DC Power Supply |
| |
===== General Setup ===== | ===== General Setup ===== |
* The [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** connects to the [[adi>en/evaluation/eval_sdp-pmod/eb.html|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) via the 120-pin connector at **J3** and is connected to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector at **J4**. | * The [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** connects to the [[adi>eval_sdp-pmod|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) via the 120-pin connector at **J3** and is connected to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector at **J4**. |
* The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] +6V power supply powers the [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** via the DC Barrel Jack of the [[adi>en/evaluation/eval_sdp-pmod/eb.html|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) at **J1**. | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] +6V power supply powers the [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** via the DC Barrel Jack of the [[adi>eval_sdp-pmod|SDP-I-PMOD]] Interposer Board (**SDP-PMOD Interposer Board**) at **J1**. |
* The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* The reference thermocouple connects to the [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** via the thermocouple connector at **+TREF-** and the tip of the thermocouple must be placed as close to **U4** as possible. | * The reference thermocouple connects to the [[adi>CN0354|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** via the thermocouple connector at **+TREF-** and the tip of the thermocouple must be placed as close to **U4** as possible. |