This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0354 [25 Jan 2021 11:09] – Fixed bad link for SDP-I-PMOD Ioana Chelaru | resources:eval:user-guides:circuits-from-the-lab:cn0354 [29 Jul 2021 07:44] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 108: | Line 108: | ||
<WRAP left round info 60%>\\ The data is exported to an Excel spreadsheet file with columns labeled accordingly. </ | <WRAP left round info 60%>\\ The data is exported to an Excel spreadsheet file with columns labeled accordingly. </ | ||
+ | \\ \\ \\ \\ \\ \\ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||