This is an old revision of the document!
CN-0352 Software User Guide
Overview
CN-0352 is a cost effective, multi-channel battery testing reference system designed for signle-cell Li-ion battery with open circuit voltage(OCV) between 3.5V to 4.4V.
It can handle charging-discharging cycle with CC(Constant Current), CV(Constant Voltage) charging mode with configurable termination control. During testing, the battery information including voltage, current and temperature are gathered, then sent and storted on PC through RS485 communication bus.
Each CN-0352 battery testing module could handle 8-channel Li-ion battery cell. With RS485 commumication bus, the testing channels could be extended upto more than hundred channels. The limitation is the communication bandwidth of RS485.
WARNING!
THIS EVALUATION SYSTEM INTERFACES TO LITHIUM ION BATTERIES WHICH CAN BE DAMAGED, CATCH ON FIRE, OR EXPLODE IF OVERCHARGED, OVER-DISCHARGED, OR SUBJECTED TO SOURCE OR SINK CURRENTS THAT EXCEED THE BATTERY MANUFACTURER’S SPECIFICATIONS. TAKE ALL NECESSARY STEPS TO PROTECT USERS DURING OPERATION.
Required Equipment
-
5
V, 5 A or higher dc power supply or wall wart(The power for battery charging of all channels is from this Power Supply).
PC or laptop with
USB Port.
USB to RS485 adapter supporting baud rate of 115200 bps.
CN0352 evaluation software (see link provided in CN0352 User Guide).
Li-ion battery cells (For safety consideration during demostration, using the Li-ion battery with integrated protection circuit is highly recommended)
Battery holder board in order to connect battery to EVAL-CN0352-EB1Z evaluation system.
Evaluation System Setup
EVAL-CN0352-EB1Z Module Setup
The EVAl-CN0352-EB1Z, battery test system in Figure below is composed of multiple I/O boards (EVAL-CN0352-EB1Z_IO) for handling the charging and discharging process, an MCU board (EVAL-CN0352-EB1Z_MCU) for battery data acquisition, testing, monitoring,and temperature management, and a backplane base board (EVAL-CN0352-EB1Z_BAS) that provides the signal interconnections between the MCU board and the multiple I/O boards.
The picture below shows all 3 type of boards and give each connector a serial number for better understanding.
See the tables below with detais of the connectors and jumpers on each board.
See the red dots on the picture. Each dot indicate the 1st pin location on the connector.
the Pin1-to-Pin1 hookup must always be done during EVAL-CN0352-EB1Z module setup process.
External Connectors
External Connectors are used to connect with external power supply, FAN, batterys and temperature sensors. It is important to connect them correctly by know the pin definition on each of them. See the table below for this information.
Connector NO. | Pin No. | Pin Name | Function | Note |
1. Power Input Connector | 1 | +5V | 5V DC Power Input | Two Pins for High Current |
2 | +5V | 5V DC Power Input | |
3 | GND | Ground | Two Pins for High Current |
4 | GND | Ground | |
2. RS485 Interface Connector | 1 | D- | Data + | |
2 | D+ | Data - | |
3 | GND | Ground | |
3. Battery Connector | 1 | B- | Power Path to Battery Cathode | 4 wire Kelvin Connection |
2 | S- | Sensing path to Battery Cathode | |
3 | S+ | Sensing path to Battery Anode | |
4 | B+ | Power Path to Battery Anode | |
4. Temperature Sensor Connector | 1 | T1 | Temperature Sensor Pin1 | Thermisor10k by 2 wire Connection |
2 | T2 | Temperature Sensor Pin2 | |
5. Reset Push Button | x | x | x | Push to reset whole system |
6. PWM FAN Connector 1 | 1 | FAN GND | FAN GND | |
2 | FAN Power | FAN Power,Connect to FAN | |
3 | Speed FB | FAN Speed feedback input | |
4 | PWM Control | FAN Speed PWM Control Output | |
7. PWM FAN Connector 2 | 1 | FAN GND | FAN GND | |
2 | FAN Power | FAN Power,Connect to FAN | |
3 | Speed FB | FAN Speed feedback input | |
4 | PWM Control | FAN Speed PWM Control Output | |
8. FAN Power Connector | 1 | FAN Power | FAN Power,Connect to 12V DC Supply | |
2 | FAN GND | FAN Power,Connect to GND of 12V Supply | |
Internal Connectors
It is necessary to have one BAS board, one MCU board and at least one I/O Board to setup the demo system. The Internal Connectors are used for EVAL-CN0352-EB1Z module setup. MCU and I/O board need to be plugged into the connectors on BAS board correctly.
Connector NO. | Function | Note |
9. | Hookup with MCU Board | Marked with JP2 on BAS board. See schematics for pin definition. |
10. | Hookup with I\O Board | Marked with P1~P8. See schematics for pin definition. |
11. | Hookup with I\O Board | Marked with S1~S8. See schematics for pin definition. |
12. | Hookup with BAS Board | Marked with J4 on MCU board. See schematics for pin definition. |
13. | Hookup with BAS Board | Marked with CNP. See schematics for pin definition. |
14. | Hookup with BAS Board | Marked with CNS. See schematics for pin definition. |
Jumpers
There are some jumpers on each board with different function listed below. See the table as a summary for the function and suggested configurations.
Jumper NO. | Configuration | Function | Note | |
15. RS485 Termination Jumper | On | 120 Ω Termination Turned on. | | |
Off | 120 Ω Termination Turned off. | Default Configuration | |
16. LK1 to LK3 on MCU Board | On | Provide Power for MCU | Always put on for correct operation | |
17. J3 on MCU Board | x | JTAG interface for MCU Debug | | |
18. JP2,JP3 on I\O Board | Both On | Connect to Battery by 4 wire Kelvin Connection | Recommended | |
Both Off | Connect to Battery by 2 wire Connection | Have lead error | |
Boards Hooking Up
The picture below shows the way to hook up the BAS, I\Os and MCU boards together. It is necessary to have at least one I/O board to make system working correctly.
EVAL-CN0352-EB1Z Demo System Setup
Connect 5V DC Power Supply to PWR connector on BAS Board;
Connect
USB to RS485 adapter to
COM connector on BAS Board;[1]
Connect the FAN to FAN1, FAN2 and FPWR connectors on BAS Board;[2]
Connect the Battery to CN1 connector on I\O board;[3-6]
Connect the Thermistor 10k sensor to CN2 on I\O board.[7]
See the picture below showing the whole CN0352 demo system.
[1] Verify the pin definition of
USB to RS485 Apapter used for communication and do a connect connection.
[2] Verify the pin definition of the FAN used for cooling and do a connect connection. Need to find a way to fix the FAN close to the Headsink on I\O board for better cooling performance. The way shown in this user guide is just for demostration and customer need to guarantee the final cooling performance in your own system.
[3] It is very dangerous to if connecting the battery with I/O board reversely.
[4] Using a battery with protection circuit integrated is highly recommended for demonstration.
[5] 4-wire Kelvin connection is recommended.
[6] There is no battery holding board in CN0352 package. Customer need to prepare the battery holding board for a good connection
[7] The default RT table if for ERTJZEG103JA, the Thermistor 10k NTC from Panisonic. If using different sensor, the RT table need to be modified to fit the new sensor.
CN0352 Evaluation Software
Software Instllation
There is a CN0352 Design Support CD in the CN0352 CftL package. Insert the CD in to your CD ROM driver and located the installation file under the location CD ROM..\CN0352 Installer\setup.exe.
Double Click the setup.exe and follow the installation wizard to install the evaluation software and drivers on your PC.
If you see the picture below, then click finish to complete the software installation.
Italic Text
Software Function Introduction
Double click the CN0352.exe, then the interface of CN0352 evaluation software shows up.
The evaluation board would send related command frame down to one or more EVAL-CN0352-EB1Z demos one the same RS485 bus regards to the button been clicked by customer. Then the EVAL-CN0352-EB1Z addressed will do related operations and may or may not send back feedback data.
System Operation Tab
Battery Scan: Do the Scan after clicked to get the ID informaiton of all the available demos that share the RS485 bus and channel ID of I\O boards on each of the demos. This is the first operation to do.
Update Config: Click this button to make current configuration shown on the software interface to become effective to all the demos on the RS485 bus.
Start Test: Click to start the test process. The testing process is a fix times of charging-discharging cycle with configured status and termination conditions. The information during testing would be gathered and stored on PC memory.
Stop Test: Click to stop the test.
Save Data: Click to save the data that already gathered on PC. The data would be processed to wirte into a xls file with specific format that could be re-imported into the software for analysis.
Import Data: Click to import the data file that had been saved by the software before.
Exit: Click to exit the software.
Channel Switching Tab
There are Battery Status and Test Procedure blocks are both refreshing to show the latest battery status that the software just received from EVAL-CN0352-EB1Z. The switching Channel Switching tab is used to switch to any of the available battery channel that customer want to look at.
: Click to switch to the
1st Battery available.
: Click to switch to the
previous Battery available.
: Switch to the expected battery channel by input the battery index.
: Click to switch to the
next Battery available.
: Click to switch to the
last Battery available.
Main Tab
Configuration Tab
For easy to do the operation and see the result, the Configuration block and Battery Status,Test Procedule on the same tab.
Battery Plots
Battery Plots showns all the battery information since the testing started. All the information are shown on the plot.
Voltage & Current Plot: This plot shows the Voltage and Current information of active battery channel.
Capacity & Temperature Plot: This plot shows the Capacity and Temperature Informaiotn of active battery channel.
Battery Summary
The Battery Summary tab listed all latest informations of each battery on one row. It is very convenient to see the any battery interested without switching the channel.
Module ID Programmer
Before doing the test, each EVAL-CN0352-EB1Z sharing the same RS485 bus need to have a unique ID. This ID is a 8-bit ID. The Default ID for the EVAL-CN0352-EB1Z is 0xFF. If there are multiple modules sharing the same RS485, than each Module need to have a different ID. This Module ID Programmer is the tools for assigning the ID.
Module ID: Input a ID number that is different with all the ID that has been assigned to other modules. The Value of Module ID will increast 1 automatically after you click the Program button and program process is succeeded.
Program: Click this button will program the module connected to RS485 bus. Only one module could be connected to RS485 bus during ID programming process.
LED: This Square LED will indicate the status of ID programming process.
Simple Testing Example
EVAL-CN0352-EB1Z Module Power On Process
EVAL-CN0352-EB1Z Module Setup. See Evaluation System Setup section for more details.
EVAL-CN0352-EB1Z Battery Testing Demo System Setup. See Evaluation System Setup section for more details.
Before Powering on the EVAL-CN0352-EB1Z Modules, break all the connection between batteries and I\O boards. It is not suggested to connect the battery to un-powered EVAL-CN0352-EB1Z module.
Plug the
USB to RS485 adapter into your PC and check to make sure that the adapter is working well and record the COM port number.
Power On All the available EVAL-CN0352-EB1Z modules
Connect batteries that you want to test to I/O boards.
Software Evaluation
Communication Setup
Open the CN0352 Evaluation software by click the CN0352.exe. This program can be found on desktop or Start Menu\All Programs\Analog Devices\CN0352.exe
Click the
COM drop down menu to selec the COM port that stand for your
USB to RS485 adapter.
Click the Baudrate drop down menu to select 11520.
IO Programm
Click the Module ID Programmer page.
If there are multiple modules, Assign a different ID to each Module.If there is only one EVAL-CN0352-EB1Z module, then you could program the module ID to 0x01 to get a quicker scaning process
Input 0x01 into Module ID test box.
Click Program button and see the LED turned on with green color.
Battery Testing
Click Configuration Tab
Click Battery Scan button to scan all the available battery channels on RS485 bus.
Click Start Test button to start batter testing with default configuration value. See the information of active battery in Battery Status & Test Procedure blocks.
Click Stop Test button to stop current testing.
Click Any of the test boxes or drop down menuses to change configurations during charging or discharging process.
Click Update Config button to download the updated configurations to the module.
do Step 3 to start testing
Click Channel Switching buttons to switch to other battery.
THIS EVALUATION SYSTEM INTERFACES TO LITHIUM
ION BATTERIES WHICH
CAN BE DAMAGED, CATCH ON
FIRE, OR EXPLODE IF OVERCHARGED, OVER-
DISCHARGED, OR SUBJECTED TO SOURCE OR SINK
CURRENTS THAT EXCEED THE BATTERY
MANUFACTURER’S SPECIFICATIONS. TAKE ALL
NECESSARY STEPS TO PROTECT USERS DURING
OPERATION