CN0348 Software User Guide
Overview
CN-0348 showcases a solution for precision 16-bit digital-to-analog conversion with wide dynamic signal range in a single supply system. It utilizes a 5V voltage reference (ADR4550), a voltage output digital-to-analog converter (AD5541A), and a rail-rail amplifier as the output buffer (ADA4500-2). The ADA4500-2 exhibits zero crossover distortion and this feature makes it an excellent choice as an output buffer to maintain the linearity of the AD5541A over its input digital code and provide a wide dynamic output range. The combination of parts provides industry-leading 16-bit integral nonlinearity (INL) of ±1LSB and differential nonlinearity (DNL) of ±1LSB with guaranteed monotonicity.
This user guide gives information on how to use the evaluation software to collect data from the EVAL-CN0348-SDPZ Daughter Board.
Required Equipment
Installing the Software
Open the file
setup.exe that is provided from the CD in kit.
NOTE: It is recommended that you install the CN0348 Evaluation Software to the default directory path C:\Program Files\Analog Devices\CN0348\ and all National Instruments products to C:\Program Files\National Instruments\
Click
Next to view the installation review page
Click Next to start the installation
Upon completion of the installation of the
CN0348 SDP Evaluation Software, the installer for the
ADI SDP Drivers will execute.
NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.
Click
“Next” to set the installation location for the
SDP Drivers.
It is recommended that you install the drivers to the default directory path
C:\Program Files\Analog Devices\SDP\DriversR2
Click “Next” to install the SDP Drivers and complete the installation of all software.
Using the Evaluation Software
Software Control and Indicator Descriptions
LDAC COntrol
Write to DAC Button
Enter the digital input code in “DIN”
When “WRITE TO DAC” button is clicked, the digital input code is sent to the DAC
Output Indicator
System Status String / LED Indicator
Code Step Control
Agilent 3458A GPIB Address Control
Current Code / Voltage Indicator
File Directory Control
INL / DNL measurement graphs
These graphs display the INL and DNL vs. input digital code when data collection is done
Transfer Function Graph
This graph shows the transfer function of the DAC output voltage vs. input digital code
SDP Board Firmware Information
Connecting the Hardware and Taking Measurements
Connect the SDP Board to the CN0348 Board
Connect +6V and analog ground to the CN0348 board (J1)
Connect the
USB cable supplied with the SDP board to the
USB port on the PC and the SDP board
Connect Vout (J3) to a multimeter
Open CN0348.exe. It should be located in C:\Program Files\Analog Devices\CN0348\
The application will attempt to connect to the board immediately
Check LDAC box
Perform functionality test by entering the following in DIN and click WRITE TO DAC
0000; multimeter should read close to 0V
FFFF; multimeter should read close to 5V
OUTPUT (Bit 15 to Bit 0) should also light up the associated LED indicator
For INL/DNL data collection:
Connect Vout to the Agilent 3458A multimeter
Connect the Agilent 3458A to the PC using a GPIB to
USB Type A connector (for data collection via Labview software)
Set the multimeter to have “NPLC” as 1
Enter GPIB Address of Agilent 3458A.
Enter desired Code Step
Code Step = 16 takes about 4min 10sec to finish measurement
Code Step = 32 takes about 2min 5sec to finish measurement
Enter the file name and path you want to save data in Enter file name to save data before running
Click on Start
Current Code and Current voltage should show the progress of measurements
To exit, go to File > Exit.
Registration
Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!