This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0346 [25 Jan 2021 11:05] – Fixed bad link for EVAL-SDP-PMOD Ioana Chelaru | resources:eval:user-guides:circuits-from-the-lab:cn0346 [29 Jul 2021 07:32] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 6: | Line 6: | ||
*One [[adi> | *One [[adi> | ||
*One [[adi> | *One [[adi> | ||
- | *One [[adi>SDP-I-PMOD|EVAL-SDP-PMOD]] Evaluation board | + | *One [[adi>EVAL_SDP-PMOD|EVAL-SDP-PMOD]] Evaluation board |
*One [[adi> | *One [[adi> | ||
*One USB Type-A plug to USB Mini-B plug cable. | *One USB Type-A plug to USB Mini-B plug cable. | ||
Line 43: | Line 43: | ||
- Input the calculated CAPDAC value into the box found at the bottom of the Calibration tab. | - Input the calculated CAPDAC value into the box found at the bottom of the Calibration tab. | ||
- {{: | - {{: | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |