This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0341 [05 Jan 2021 16:25] Ioana Chelaru Removed old references |
resources:eval:user-guides:circuits-from-the-lab:cn0341 [29 Jul 2021 07:30] Harvey John De Chavez Hardware Registration |
||
---|---|---|---|
Line 58: | Line 58: | ||
- The image below displays one last common error source, sensor-to-magnet distance. The ideal distance between the sensor and magnet is half of the magnet length. Increasing or decreasing this distance introduces errors into the measurement. | - The image below displays one last common error source, sensor-to-magnet distance. The ideal distance between the sensor and magnet is half of the magnet length. Increasing or decreasing this distance introduces errors into the measurement. | ||
- {{ :resources:eval:user-guides:circuits-from-the-lab:cn0341:img_0350.jpg?800 |}} | - {{ :resources:eval:user-guides:circuits-from-the-lab:cn0341:img_0350.jpg?800 |}} | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0341-SDPZ?&v=RevA|Register]] to receive all these great benefits and more! | ||
+ | </WRAP> |