This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0336 [01 Oct 2013 21:58] – complete Christo Hrisulev | resources:eval:user-guides:circuits-from-the-lab:cn0336 [07 Jun 2018 08:51] – Jesse Daniel Santos | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0336 Software User Guide ====== | ====== CN0336 Software User Guide ====== | ||
===== Overview===== | ===== Overview===== | ||
- | [[http:// | + | [[ADI>CN0336]] provides robust and complete solution for 4 mA-to-20 mA current to digital conversion with isolation, for wide variety measurements where, sensors with standard 4-20 mA output are used. The design solution is optimized for high precision and low cost measurement, |
- | The circuit shown in Figure 1 incorporates [[http:// | + | The circuit shown in Figure 1 incorporates [[ADI>AD8606ARZ]] OpAmp, [[ADI>AD7091RBRMZ]] 12-bit successive approximation (SAR) ADC, and [[ADI>ADuM5401ARWZ]] isolator to create a standard 4 mA-to-20mA current measurement system. |
The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | ||
- | This [[http:// | + | This [[ADI>CN0336]] circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. |
The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[http:// | The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[http:// | ||
Line 10: | Line 10: | ||
{{ : | {{ : | ||
+ | |||
+ | Figure 1. 4 mA to 20 mA Single Supply Analog to Digital Conversion with Isolation (All Connections and Decoupling Not Shown) | ||