This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0326 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0326 [29 Jul 2021 07:24] – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 127: | Line 127: | ||
- When choosing the custom buffer solution table, navigate through the panel that contains the file that will be used for temperature compensation. | - When choosing the custom buffer solution table, navigate through the panel that contains the file that will be used for temperature compensation. | ||
- After choosing the source of the buffer solution temperature coefficient table, click Calibration Point 2 button to set the third point of calibration. | - After choosing the source of the buffer solution temperature coefficient table, click Calibration Point 2 button to set the third point of calibration. | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||