This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Next revision Both sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0326 [03 Jan 2021 21:55] Robin Getz fix links |
resources:eval:user-guides:circuits-from-the-lab:cn0326 [29 Jul 2021 07:24] Harvey John De Chavez Hardware Registration |
||
---|---|---|---|
Line 127: | Line 127: | ||
- When choosing the custom buffer solution table, navigate through the panel that contains the file that will be used for temperature compensation. (Note: a sample format of a table can be found in CN0326 Design Support Package with a folder name NIST Buffer Solution Table Format) | - When choosing the custom buffer solution table, navigate through the panel that contains the file that will be used for temperature compensation. (Note: a sample format of a table can be found in CN0326 Design Support Package with a folder name NIST Buffer Solution Table Format) | ||
- After choosing the source of the buffer solution temperature coefficient table, click Calibration Point 2 button to set the third point of calibration. | - After choosing the source of the buffer solution temperature coefficient table, click Calibration Point 2 button to set the third point of calibration. | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0326-PMDZ?&v=RevB|Register]] to receive all these great benefits and more! | ||
+ | </WRAP> | ||