Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0303 [11 Oct 2016 19:16]
Brandon Bushey [Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ]
resources:eval:user-guides:circuits-from-the-lab:cn0303 [29 Jul 2021 07:22] (current)
Harvey John De Chavez Hardware Registration
Line 1: Line 1:
 ====== Vibration Analysis (CN0303) ====== ====== Vibration Analysis (CN0303) ======
 +
 +{{page>/​wiki/​common#​retired&​nofooter&​noheader}}
 +
 +An [[adi>​media/​en/​reference-design-documentation/​reference-designs/​CN0303.pdf|archive]] of the circuit note.
  
 ===== Overview ===== ===== Overview =====
Line 5: Line 9:
  
 ===== General Setup ===== ===== General Setup =====
-  *One [[http://​www.analog.com/​CN0303|EVAL-CN0303-SDPZ]] Evaluation Board +  *One EVAL-CN0303-SDPZ Evaluation Board 
-  *One [[http://​www.analog.com/​en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001]] Evaluation Board +  *One [[adi>en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001]] Evaluation Board 
-  *[[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation board +  *[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation board 
-  *[[ftp://​ftp.analog.com/​pub/​cftl/​CN0303|CN0303 Evaluation Software]]+  *CN0303 Evaluation Software
   *One 6V wallwart. ​ (EVAL-CFTL-6V-PWRZ)   *One 6V wallwart. ​ (EVAL-CFTL-6V-PWRZ)
   *One DC power supply with a 0-6V output. ​ (HP6236B) ​   *One DC power supply with a 0-6V output. ​ (HP6236B) ​
Line 38: Line 42:
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​eval-adxl001.jpg?​ |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​eval-adxl001.jpg?​ |}}
 ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ =====
-  - First, connect the discrete female colored cable to connector P1 of the [[http://​www.analog.com/​en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001-70BEZ]]. +  - First, connect the discrete female colored cable to connector P1 of the [[adi>en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001-70BEZ]]. 
-  - Secondly, connect the discrete female colored cable to connector J6 of the [[http://​www.analog.com/​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]].{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB.jpg?​ |}} +  - Secondly, connect the discrete female colored cable to connector J6 of the EVAL-CN0303-SDPZ.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB.jpg?​ |}} 
-  - Connect the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the [[http://​www.analog.com/​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. +  - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the EVAL-CN0303-SDPZ PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. 
-  - Plug in the DC barrel jack to connector J5 of the [[http://​www.analog.com/​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] and the mini end of the USB cable into connector J1 of the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.+  - Plug in the DC barrel jack to connector J5 of the EVAL-CN0303-SDPZ and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB + Cables.jpg? |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB + Cables.jpg? |}}
  
Line 51: Line 55:
   - The following is a list of all available software controls found in the **Acceleration Results** tab, grouped according to their location in the software:   - The following is a list of all available software controls found in the **Acceleration Results** tab, grouped according to their location in the software:
     - **System Controls**     - **System Controls**
-      - **Connect** – This button configures the [[http://​www.analog.com/​ad7476|AD7476]] by writing to the necessary registers.  ​+      - **Connect** – This button configures the [[adi>ad7476|AD7476]] by writing to the necessary registers.  ​
       - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized.       - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized.
     - **Data Acquisition Controls**     - **Data Acquisition Controls**
Line 59: Line 63:
       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', '​Pk-to-Pk Codes',​ '​Pk-to-Pk Volts' etc.       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', '​Pk-to-Pk Codes',​ '​Pk-to-Pk Volts' etc.
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​software_-_frequency_results_tab.png |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​software_-_frequency_results_tab.png |}}
 +
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0303-SDPZ?&​v=RevA|Register]] to receive all these great benefits and more!
 +</​WRAP>​
resources/eval/user-guides/circuits-from-the-lab/cn0303.1476206162.txt.gz · Last modified: 11 Oct 2016 19:16 by Brandon Bushey