This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0303 [05 Jan 2021 16:45] Ioana Chelaru Removed bad link for CN0303 |
resources:eval:user-guides:circuits-from-the-lab:cn0303 [29 Jul 2021 07:22] (current) Harvey John De Chavez Hardware Registration |
||
---|---|---|---|
Line 1: | Line 1: | ||
====== Vibration Analysis (CN0303) ====== | ====== Vibration Analysis (CN0303) ====== | ||
+ | |||
+ | {{page>/wiki/common#retired&nofooter&noheader}} | ||
+ | |||
+ | An [[adi>media/en/reference-design-documentation/reference-designs/CN0303.pdf|archive]] of the circuit note. | ||
===== Overview ===== | ===== Overview ===== | ||
Line 39: | Line 43: | ||
===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== | ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== | ||
- First, connect the discrete female colored cable to connector P1 of the [[adi>en/mems-sensors/mems-inertial-sensors/adxl001/products/EVAL-ADXL001/eb.html|ADXL001-70BEZ]]. | - First, connect the discrete female colored cable to connector P1 of the [[adi>en/mems-sensors/mems-inertial-sensors/adxl001/products/EVAL-ADXL001/eb.html|ADXL001-70BEZ]]. | ||
- | - Secondly, connect the discrete female colored cable to connector J6 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]].{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB.jpg? |}} | + | - Secondly, connect the discrete female colored cable to connector J6 of the EVAL-CN0303-SDPZ.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB.jpg? |}} |
- | - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. | + | - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the EVAL-CN0303-SDPZ PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. |
- | - Plug in the DC barrel jack to connector J5 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC. | + | - Plug in the DC barrel jack to connector J5 of the EVAL-CN0303-SDPZ and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC. |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB + Cables.jpg? |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB + Cables.jpg? |}} | ||
Line 59: | Line 63: | ||
- **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', 'Pk-to-Pk Codes', 'Pk-to-Pk Volts' etc. | - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', 'Pk-to-Pk Codes', 'Pk-to-Pk Volts' etc. | ||
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:software_-_frequency_results_tab.png |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:software_-_frequency_results_tab.png |}} | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0303-SDPZ?&v=RevA|Register]] to receive all these great benefits and more! | ||
+ | </WRAP> |