Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0303 [05 Jan 2021 16:45]
Ioana Chelaru Removed bad link for CN0303
resources:eval:user-guides:circuits-from-the-lab:cn0303 [29 Jul 2021 07:22]
Harvey John De Chavez Hardware Registration
Line 1: Line 1:
 ====== Vibration Analysis (CN0303) ====== ====== Vibration Analysis (CN0303) ======
 +
 +{{page>/​wiki/​common#​retired&​nofooter&​noheader}}
 +
 +An [[adi>​media/​en/​reference-design-documentation/​reference-designs/​CN0303.pdf|archive]] of the circuit note.
  
 ===== Overview ===== ===== Overview =====
Line 39: Line 43:
 ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ =====
   - First, connect the discrete female colored cable to connector P1 of the [[adi>​en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001-70BEZ]].   - First, connect the discrete female colored cable to connector P1 of the [[adi>​en/​mems-sensors/​mems-inertial-sensors/​adxl001/​products/​EVAL-ADXL001/​eb.html|ADXL001-70BEZ]].
-  - Secondly, connect the discrete female colored cable to connector J6 of the [[adi>​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]].{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB.jpg?​ |}} +  - Secondly, connect the discrete female colored cable to connector J6 of the EVAL-CN0303-SDPZ.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB.jpg?​ |}} 
-  - Connect the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the [[adi>​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. +  - Connect the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the EVAL-CN0303-SDPZ PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. 
-  - Plug in the DC barrel jack to connector J5 of the [[adi>​eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] and the mini end of the USB cable into connector J1 of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.+  - Plug in the DC barrel jack to connector J5 of the EVAL-CN0303-SDPZ and the mini end of the USB cable into connector J1 of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB + Cables.jpg? |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​PCB + Cables.jpg? |}}
  
Line 59: Line 63:
       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', '​Pk-to-Pk Codes',​ '​Pk-to-Pk Volts' etc.       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', '​Pk-to-Pk Codes',​ '​Pk-to-Pk Volts' etc.
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​software_-_frequency_results_tab.png |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0303:​software_-_frequency_results_tab.png |}}
 +
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0303-SDPZ?&​v=RevA|Register]] to receive all these great benefits and more!
 +</​WRAP>​
resources/eval/user-guides/circuits-from-the-lab/cn0303.txt · Last modified: 29 Jul 2021 07:22 by Harvey John De Chavez