Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0301 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0301 [29 Jul 2021 07:21] (current) – Hardware Registration Harvey John De Chavez |
---|
* [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] Evaluation Board (**CN-0301 Board**) | * [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] Evaluation Board (**CN-0301 Board**) |
* [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent |
* [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties, Inc. E-100 Economy Series LVDT) | * [[adi>CN0301|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties, Inc. E-100 Economy Series LVDT) |
* [[ftp://ftp.analog.com/pub/cftl/CN0301/|CN-0301 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0301/|CN-0301 Evaluation Software]] |
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) |
* The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack |
* The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* The [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**. | * The [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**. |
\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-test_setup.png?nolink&|}} | \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-test_setup.png?nolink&|}} |
| |
---- | ---- |
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== |
- Connect the [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware.png?600|}}\\ \\ | - Connect the [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware.png?600|}}\\ \\ |
- Connect **J8** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware2.png?600|}}\\ \\ | - Connect **J8** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware2.png?600|}}\\ \\ |
- Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware3.png?600|}}\\ \\ | - Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware3.png?600|}}\\ \\ |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:functionsexplained.zip|API Functions Explained}} | {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:functionsexplained.zip|API Functions Explained}} |
| |
| =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0301-SDPZ?&v=RevC|Register]] to receive all these great benefits and more! |
| </WRAP> |