This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0301 [10 Feb 2021 14:50] Robin Getz fix links |
resources:eval:user-guides:circuits-from-the-lab:cn0301 [29 Jul 2021 07:21] (current) Harvey John De Chavez Hardware Registration |
||
---|---|---|---|
Line 29: | Line 29: | ||
* The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack | ||
* The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | ||
- | * The [[adi>CN301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**. | + | * The [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**. |
\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-test_setup.png?nolink&|}} | \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-test_setup.png?nolink&|}} | ||
Line 44: | Line 44: | ||
---- | ---- | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect the [[adi>CN301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware.png?600|}}\\ \\ | + | - Connect the [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware.png?600|}}\\ \\ |
- Connect **J8** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware2.png?600|}}\\ \\ | - Connect **J8** of the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware2.png?600|}}\\ \\ | ||
- Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware3.png?600|}}\\ \\ | - Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:cn0301-hardware3.png?600|}}\\ \\ | ||
Line 138: | Line 138: | ||
{{:resources:eval:user-guides:circuits-from-the-lab:cn0301:functionsexplained.zip|API Functions Explained}} | {{:resources:eval:user-guides:circuits-from-the-lab:cn0301:functionsexplained.zip|API Functions Explained}} | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0301-SDPZ?&v=RevC|Register]] to receive all these great benefits and more! | ||
+ | </WRAP> |