Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0301 [10 Feb 2021 14:50]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0301 [29 Jul 2021 07:21]
Harvey John De Chavez Hardware Registration
Line 29: Line 29:
   * The [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack   * The [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack
   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
-  * The [[adi>CN301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**.+  * The [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**.
 \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-test_setup.png?​nolink&​|}} \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-test_setup.png?​nolink&​|}}
  
Line 44: Line 44:
 ---- ----
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
-  - Connect the [[adi>CN301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>​**NOTE:​** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties,​ Inc the wiring schematic will be different!</​WRAP>​\\ \\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_table.png?​nolink&​ |}}{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_schematic.png?​|nolink}}\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware.png?​600|}}\\ \\ +  - Connect the [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>​**NOTE:​** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties,​ Inc the wiring schematic will be different!</​WRAP>​\\ \\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_table.png?​nolink&​ |}}{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_schematic.png?​|nolink}}\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware.png?​600|}}\\ \\ 
   - Connect **J8** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware2.png?​600|}}\\ \\    - Connect **J8** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware2.png?​600|}}\\ \\ 
   - Connect the [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware3.png?​600|}}\\ \\   - Connect the [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware3.png?​600|}}\\ \\
Line 138: Line 138:
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​functionsexplained.zip|API Functions Explained}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​functionsexplained.zip|API Functions Explained}}
  
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0301-SDPZ?&​v=RevC|Register]] to receive all these great benefits and more!
 +</​WRAP>​
resources/eval/user-guides/circuits-from-the-lab/cn0301.txt · Last modified: 29 Jul 2021 07:21 by Harvey John De Chavez