Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0301 [03 Jan 2021 21:55]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0301 [11 Feb 2021 16:20]
Ioana Chelaru
Line 16: Line 16:
   * [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] Evaluation Board (**CN-0301 Board**)   * [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] Evaluation Board (**CN-0301 Board**)
   * [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent   * [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent
-  * [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties,​ Inc. E-100 Economy Series LVDT) +  * [[adi>CN0301|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties,​ Inc. E-100 Economy Series LVDT) 
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0301/​|CN-0301 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0301/​|CN-0301 Evaluation Software]]
     * (supplied with provided CD in kit)     * (supplied with provided CD in kit)
Line 29: Line 29:
   * The [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack   * The [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the DC barrel jack
   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
-  * The [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**.+  * The [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** via the 6-pin header at **J1**.
 \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-test_setup.png?​nolink&​|}} \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-test_setup.png?​nolink&​|}}
  
Line 44: Line 44:
 ---- ----
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
-  - Connect the [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>​**NOTE:​** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties,​ Inc the wiring schematic will be different!</​WRAP>​\\ \\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_table.png?​nolink&​ |}}{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_schematic.png?​|nolink}}\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware.png?​600|}}\\ \\ +  - Connect the [[adi>CN0301|EVAL-CFTL-LVDT]] **(LVDT)** to **J1** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>​**NOTE:​** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties,​ Inc the wiring schematic will be different!</​WRAP>​\\ \\ \\ \\ \\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_table.png?​nolink&​ |}}{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-wiring_schematic.png?​|nolink}}\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware.png?​600|}}\\ \\ 
   - Connect **J8** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware2.png?​600|}}\\ \\    - Connect **J8** of the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)** to **CON A** of the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware2.png?​600|}}\\ \\ 
   - Connect the [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware3.png?​600|}}\\ \\   - Connect the [[adi>​EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J3** on the [[adi>​EVAL-CN0301-SDPZ|EVAL-CN0301-SDPZ]] **(CN-0301 Board)**\\ \\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0301:​cn0301-hardware3.png?​600|}}\\ \\
resources/eval/user-guides/circuits-from-the-lab/cn0301.txt · Last modified: 29 Jul 2021 07:21 by Harvey John De Chavez