CN-0296 Software User Guide
OVERVIEW
CN-0296 is a low cost high performance sound bar system that can accept an analog stereo audio signal as an input and can output up to eight channels of audio with discrete processing on each channel. The circuit is ideal for small docking stations and portable media devices. The circuit offers low power consumption and high efficiency operation without sacrificing audio quality. The circuit is also capable of driving headphones without the need of additional components.
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing, also called SigmaDSP®. It has two ADCs to accept two audio channels and can apply digital processing with the integrated SigmaDSP® core.
SigmaDSP® processors are optimized for audio applications and programmed using SigmaStudio development software for ease of use and faster development. Its output can send up to eight channels of digital audio data to the output amplifiers using the serial interface. It allows different audio signal processing in each channel, such as volume control, custom equilization, filtering, and spatialization effects tuned to the specific speaker configuration.The ADAU1761 processes and converts analog audio to digital format and drives the SSM2518 power amplifier.
The SSM2518 is a digital input class-D audio power amplifier that can output two channels of audio with a continuous power of 2 watts each into a 4 Ωload. Its channel-mapping feature allows it to select the specific channel to output among those that are available in the interface. This makes it ideal for surround sound applications.
GENERAL SETUP
MINIMUM PC/SYSTEM REQUIREMENTS
HOW TO INSTALL THE EVALUATION SOFTWARE
Extract the file
CN0296 Eval Software.zip and open the file
setup.exe.
NOTE: It is recommended that you install the CN0296 Evaluation Software to the default directory path C:\Program Files\Analog Devices\CN0296\ and all National Instruments products to C:\Program Files\National Instruments\
Click
Next to view the installation review page
Click
Next to start the installation
Upon completion of the installation of the
CN0296 Evaluation Software, the installer for the
ADI SDP Drivers will execute.
NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.

Press
“Next” to set the installation location for the
SDP Drivers.
It is recommended that you install the drivers to the default directory path
C:\Program Files\Analog Devices\SDP\Drivers
Press
“Next” to install the
SDP Drivers and complete the installation of all software. Click
“Finish” when done.

STEP BY STEP INSTRUCTION FOR CONNECTING THE HARDWARE
Connect the 120-pin connector on the
EVAL-CN0296-SDPZ circuit board to the connector marked “CON A” on the
EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.
Plug the mini end of the
USB cable into connector
J2 of the
EVAL-SDP-CB1Z and connect the other end of the
USB cable into the Laptop or PC.
-
Populate a jumper across P6 and P11 as depicted in the picture above
Connect speakers in the designated male headers
OPENING AND ENABLING THE EVALUATION SOFTWARE
Launch the executable found at C:\Program Files\Analog Devices\CN0296 and press the “Connect” button.
After pressing the “Connect” button, a prompt will appear informing the user if the SDP is already connected.
Press the “Play Soundbar” button in order to start using the functions of the soundbar.
USING THE EVALUATION SOFTWARE
Below are the list of available software controls grouped according to their location int he software
GUI:
System Controls
Connect - configures the
ADAU1761 and
SSM2518 by writing the necessary registers. THe display label at the bottom of the
GUI will provide a prompt once the soundbar is configured properly.
Configuration
Play Soundbar - writes the preconfigured algorithms in ADAU1761 registers to enable it to demonstrate the
ADI Effects
ADI Effects - preconfigured algorithms from SigmaStudio
None - Resets the soundbar to implement no special algorithms
Spatializer - an advanced algorithm that allows for a wider stereo image to be played back from two closely spaced speakers. This spatializer algorithm is only meant to widen signals that are already in stereo format, in order to enhance the image. The function is similar to the Phat-Stereo algorithm but performs a more advanced implementation of the algorithm to achieve a better effect. .
Superbass - provides input-level dependent bass boost. Lower level signals are boosted more than higher-amplitude signals. Using a variable-Q filter, this algorithm dynamically adjusts the amount of boost.
Loudness - amplifies lower level and higher level amplitude signals to maximize the volume range.
Test tone - Provides a 1-KHz test tone when to test the board even in the absence of an input signal
Volume, Bass, Treble Controls - provides adjustable volume, bass and treble levels of the input signal
Channel Mute Control - enables and disable the eight channels individually or collectively.
Advanced Configuration
Configure ADAU1761 - configures the ADAU1761 using user-defined algorithms from Sigmastudio.
Firmware Version - provides details on the firmware version of the Blackfin used by the SDP board.
Registration
Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!