Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0295 [09 Jan 2021 00:32] – user interwiki links Robin Getzresources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] (current) – Hardware Registration Harvey John De Chavez
Line 34: Line 34:
  
   - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB.   - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB.
-  - A differential sensor gauge like from [[https://sensing.honeywell.com/index.php?ci_id=45106|Honeywell]] or from [[http://www.nxp.com/products/sensors/pressure-sensors:DRSNSPRSSR|NXP]] can be used for evaluation. +  - A differential sensor gauge like from [[http://www.nxp.com/products/sensors/pressure-sensors:DRSNSPRSSR|NXP]] which can be used for evaluation. 
 <note note> <note note>
   * Vsense is where the analog voltage output of the sensor is being taken for measurement.  Pin polarity should be take into account.   * Vsense is where the analog voltage output of the sensor is being taken for measurement.  Pin polarity should be take into account.
Line 107: Line 107:
 </WRAP> </WRAP>
  
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0295-EB1Z?&v=RevD|Register]] to receive all these great benefits and more!
 +</WRAP>
 // End of Document // // End of Document //
resources/eval/user-guides/circuits-from-the-lab/cn0295.txt · Last modified: 29 Jul 2021 07:17 by Harvey John De Chavez