This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0295 [09 Jan 2021 00:32] Robin Getz user interwiki links |
resources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] Harvey John De Chavez Hardware Registration |
||
---|---|---|---|
Line 34: | Line 34: | ||
- A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | ||
- | - A differential sensor gauge like from [[https://sensing.honeywell.com/index.php?ci_id=45106|Honeywell]] or from [[http://www.nxp.com/products/sensors/pressure-sensors:DRSNSPRSSR|NXP]] can be used for evaluation. | + | - A differential sensor gauge like from [[http://www.nxp.com/products/sensors/pressure-sensors:DRSNSPRSSR|NXP]] which can be used for evaluation. |
<note note> | <note note> | ||
* Vsense is where the analog voltage output of the sensor is being taken for measurement. Pin polarity should be take into account. | * Vsense is where the analog voltage output of the sensor is being taken for measurement. Pin polarity should be take into account. | ||
Line 107: | Line 107: | ||
</WRAP> | </WRAP> | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0295-EB1Z?&v=RevD|Register]] to receive all these great benefits and more! | ||
+ | </WRAP> | ||
// End of Document // | // End of Document // |