Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0287 [29 Jul 2021 06:08] – Hardware Registration Harvey John De Chavezresources:eval:user-guides:circuits-from-the-lab:cn0287 [15 Aug 2022 04:18] (current) Allan Uy
Line 9: Line 9:
 Input transient and overvoltage protection are provided by low leakage transient voltage supressors (TVS) and Schottky diodes. The SPI-compatible digital inputs and outputs are isolated (2500 V rms), and the circuit is operated on a fully isolated power supply.  Input transient and overvoltage protection are provided by low leakage transient voltage supressors (TVS) and Schottky diodes. The SPI-compatible digital inputs and outputs are isolated (2500 V rms), and the circuit is operated on a fully isolated power supply. 
  
-[[adi>CN0287|EVAL-CN0287-SDPZ]] Daughter Board. 
  
-{{:resources:eval:user-guides:circuits-from-the-lab:CN0287:cn0287_00_1024_81_.png?700}}+{{:resources:eval:user-guides:circuits-from-the-lab:CN0287:cn0287_00_1024_81_.png?600}}
  
  
Line 19: Line 18:
   * [[adi>EVAL-CN0287-SDPZ|EVAL-CN0287-SDPZ]] Evaluation Board (**CN-0287 Board**)   * [[adi>EVAL-CN0287-SDPZ|EVAL-CN0287-SDPZ]] Evaluation Board (**CN-0287 Board**)
   * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent   * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent
-  * [[ftp://ftp.analog.com/pub/cftl/CN0287/|CN-0287 Evaluation Software]] +  * [[https://swdownloads.analog.com/cse/cftl/CN0287/1.0.2/CN0287_Evaluation_Software.zip|CN0287 Evaluation Software]]
-    * (supplied with provided CD in kit)+
   * PC with the following //Minimum Requirements//   * PC with the following //Minimum Requirements//
     * Windows XP Service Pack 2 (32-bit)     * Windows XP Service Pack 2 (32-bit)
Line 39: Line 37:
   * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.   * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
  
-Block diagram image here\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0287:hardware_connection_with_label.png?direct&700|}}\\ +\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0287:hardware_connection_with_label.png?direct&700|}}\\ 
  
 ---- ----
 ===== Installing the Software ===== ===== Installing the Software =====
  
-  - Extract the file **CN0287 SDP Evaluation Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 55%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0287/|CN0287 SDP Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0287\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_1.png?direct&600|}}+  - Extract the file **CN0287 SDP Evaluation Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 55%>**NOTE:** It is recommended that you install the [[https://swdownloads.analog.com/cse/cftl/CN0287/1.0.2/CN0287_Evaluation_Software.zip|CN0287 Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0287\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_1.png?direct&600|}}
   - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_2.png?direct&600|}}\\ \\    - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_2.png?direct&600|}}\\ \\ 
   - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_3.png?direct&600|}}\\ \\    - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:CN0287:software_installation_3.png?direct&600|}}\\ \\ 
resources/eval/user-guides/circuits-from-the-lab/cn0287.txt · Last modified: 15 Aug 2022 04:18 by Allan Uy