This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0269 [15 Oct 2013 11:32] – [Capturing a Single Capture] yue hua | resources:eval:user-guides:circuits-from-the-lab:cn0269 [29 Jul 2021 05:56] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | |||
- | } | ||
====== CN-0269 Software User Guide ====== | ====== CN-0269 Software User Guide ====== | ||
+ | |||
===== Overview ===== | ===== Overview ===== | ||
- | [[http:// | + | [[adi>CN0287|CN-0269]] is a high performance industrial signal level multi-channel data acquisition circuit that can process 16-channels of single-ended inputs or 8-channels of differential inputs with up to 18-bit resolution. |
A single channel can be sampled at up to 1.33 MSPS with 18-bit resolution. A channel-to-channel switching rate of 250 kHz between all input channels provides 16-bit performance. | A single channel can be sampled at up to 1.33 MSPS with 18-bit resolution. A channel-to-channel switching rate of 250 kHz between all input channels provides 16-bit performance. | ||
Line 11: | Line 10: | ||
\\ {{ : | \\ {{ : | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] Daughter Board (**CN0269 Board**) |
- | * [[http:// | + | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 24: | Line 23: | ||
* Signal Generator for Sin Wave with +/-10V Vpp and frequency upto 500KHz | * Signal Generator for Sin Wave with +/-10V Vpp and frequency upto 500KHz | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The **[[http:// | + | * The **[[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]** Board connects to the **[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board via the 120-Pin connector |
- | * The DC Power Supply +6V Output connects to **CN2** on **[[http:// | + | * The DC Power Supply +6V Output connects to **CN2** on **[[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]**, |
- | * The **[[http:// | + | * The **[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board connects to the PC via the USB cable.\\ {{: |
===== Installing the Software ===== | ===== Installing the Software ===== | ||
Line 39: | Line 38: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect **J1** of the [[http:// | + | - Connect **J1** of the [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)\\ |
- | - Set the JP3 and JP4 on [[http:// | + | - Set the JP3 and JP4 on [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to select the input range and Connect the signal correctly according to the pin definition.\\ \\ {{: |
- Connect the USB Cable to the SDP-B Board and leave the other side of the cable unconnected. | - Connect the USB Cable to the SDP-B Board and leave the other side of the cable unconnected. | ||
- Connect the 6V DC power to CN2 and +/-12V DC power to CN1 and Turn on the DC power supply to power up the board. | - Connect the 6V DC power to CN2 and +/-12V DC power to CN1 and Turn on the DC power supply to power up the board. | ||
Line 54: | Line 53: | ||
* When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. A connection to the SDP-B Board must be made to use the software. | * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. A connection to the SDP-B Board must be made to use the software. | ||
- **Start Acquisition Button** | - **Start Acquisition Button** | ||
- | * When this button is pressed, the SDP-B Board starts to acquire data from **[[http:// | + | * When this button is pressed, the SDP-B Board starts to acquire data from **[[adi>CN0269|EVAL-CN0269-SDPZ]]** Board. |
- **Save Data Button** | - **Save Data Button** | ||
* When this button is pressed, the SDP-B Board save the data into the same directory where the application is installed.\\ \\ <WRAP left round important box 50%> | * When this button is pressed, the SDP-B Board save the data into the same directory where the application is installed.\\ \\ <WRAP left round important box 50%> | ||
- **Control Tabs** | - **Control Tabs** | ||
- | * __Configuration Tab__: All the configuration items through [[http:// | + | * __Configuration Tab__: All the configuration items through [[adi>en/ |
* __Multi-Channel Tab__: This tab shows all the signals on one tab which is convenient to compare the signals from different channels. More details about **Multi-Channel Tab** will be introduced in the following Section. | * __Multi-Channel Tab__: This tab shows all the signals on one tab which is convenient to compare the signals from different channels. More details about **Multi-Channel Tab** will be introduced in the following Section. | ||
* __Single Channel Tab__: This tab shows the specific channel which is more clearer than Multi-Channel Tab. More details about **Single Channel Tab** will be introduced in the following Section. | * __Single Channel Tab__: This tab shows the specific channel which is more clearer than Multi-Channel Tab. More details about **Single Channel Tab** will be introduced in the following Section. | ||
- | * __SDP Information__: | + | * __SDP Information__: |
- **Configuration Items** | - **Configuration Items** | ||
- | * All the items that used to control **[[http:// | + | * All the items that used to control **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board. |
- **Hardware Configuration Diagram** | - **Hardware Configuration Diagram** | ||
* This picture block shows the way of hardware configuration in terms of jumper setting and signal connection according to the current configuration. | * This picture block shows the way of hardware configuration in terms of jumper setting and signal connection according to the current configuration. | ||
Line 76: | Line 75: | ||
* The options are “Connector A” or “Connector B”. The connector to be used must be selected before clicking the **Connect Button**. | * The options are “Connector A” or “Connector B”. The connector to be used must be selected before clicking the **Connect Button**. | ||
* __**Signal Range Dropdown Menu**__ | * __**Signal Range Dropdown Menu**__ | ||
- | * This control will select acceptable input range of **[[http:// | + | * This control will select acceptable input range of **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board. After selecting the input range, customer need to make the hardware configuration according the way shown in the **Hardware Configuration Diagram**. |
* The options are -10V to +10V or -5V to +5V. | * The options are -10V to +10V or -5V to +5V. | ||
* __**Signal Type Dropdown Menu**__ | * __**Signal Type Dropdown Menu**__ | ||
- | * //8 Channels, Differential//: | + | * //8 Channels, Differential//: |
- | * //16 Channels, Single-Ended//: | + | * //16 Channels, Single-Ended//: |
* __**Acquisition Mode Dropdown Menu**__ | * __**Acquisition Mode Dropdown Menu**__ | ||
- | * //Single Channel//: When this mode is selected, the Evaluation Software would control **[[http:// | + | * //Single Channel//: When this mode is selected, the Evaluation Software would control **[[adi>en/ |
- | * //All Channel Scan//: When this mode is selected, the Evaluation Software would control **[[http:// | + | * //All Channel Scan//: When this mode is selected, the Evaluation Software would control **[[adi>en/ |
* __**Select the Channel Dropdown Menu**__ | * __**Select the Channel Dropdown Menu**__ | ||
* This control is shown on the **configuration tab** only when the **Acquisition Mode** is " | * This control is shown on the **configuration tab** only when the **Acquisition Mode** is " | ||
Line 128: | Line 127: | ||
* This Sub Tab shows the distribution status in time domain for the selected channel. | * This Sub Tab shows the distribution status in time domain for the selected channel. | ||
- **Dynamic Performance Analysis** | - **Dynamic Performance Analysis** | ||
- | * SNR: Signal | + | * SNR: Usually, the SNR is the ratio of the rms value of the actual input signal |
* SINAD: Signal-to-Noise-and-Distortion Ratio. | * SINAD: Signal-to-Noise-and-Distortion Ratio. | ||
* SFDR: Spurious Free Dynamic Range. | * SFDR: Spurious Free Dynamic Range. | ||
* THD: Total Harmonic Distortion. | * THD: Total Harmonic Distortion. | ||
- | * Sin/ | + | * Sin/ |
* Fund ampl: Fundamental Frequency Amplitude. | * Fund ampl: Fundamental Frequency Amplitude. | ||
Line 156: | Line 155: | ||
- Click the **Start Acquisition**. | - Click the **Start Acquisition**. | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||