This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0254 [15 Dec 2017 22:51] – Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0254 [03 Jan 2021 21:56] – fix links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* DC Power Supply (6 V, 500 mA) | * DC Power Supply (6 V, 500 mA) | ||
Line 26: | Line 26: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0254-SDPZ|EVAL-CN0254-SDPZ]] **(CN-0254 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **CN2** is the +6 V power supply input | * Terminal block **CN2** is the +6 V power supply input | ||
* Terminal block **J2** is for the multiple channels analog input | * Terminal block **J2** is for the multiple channels analog input | ||
Line 34: | Line 34: | ||
==== Test setup ==== | ==== Test setup ==== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- After setting the dc output supply to 6 V output, turn the supply off | - After setting the dc output supply to 6 V output, turn the supply off | ||
- With power to the supply off, connect 6 V to CN2 | - With power to the supply off, connect 6 V to CN2 | ||
Line 121: | Line 121: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout |