This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0241 [15 Sep 2017 10:23] – Trecia Agoylo | resources:eval:user-guides:circuits-from-the-lab:cn0241 [20 Nov 2023 04:18] (current) – Deprecated Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======CN0241 High-Side Current Sensing with Input Overvoltage Protection====== | + | ======CN0241 |
+ | |||
+ | |||
+ | <note important> | ||
===== Overview ===== | ===== Overview ===== | ||
- | High-side current monitors are likely to encounter overvoltage conditions from transients or when the monitoring circuits are connected, disconnected, | + | High-side current monitors are likely to encounter overvoltage conditions from transients or when the monitoring circuits are connected, disconnected, |
+ | |||
+ | The circuit is powered by the [[ADI> | ||
+ | |||
+ | This applies voltage to the inputs of the unpowered ADA4096-2; however, no latch-up or damage occurs for input voltages up to 32V. If slower throughput rates are required, the [[ADI> | ||
- | The circuit is powered by the [[ADI> | + | {{ : |
- | This applies voltage to the inputs of the unpowered ADA4096-2; however, no latch-up or damage occurs for input voltages up to 32V. If slower throughput rates are required, the [[ADI> | ||
- | {{ : | ||
- | ---- | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[ADI> | * [[ADI> | ||
Line 17: | Line 21: | ||
* DC power supply capable of driving 5 V/2.5 A | * DC power supply capable of driving 5 V/2.5 A | ||
* 2 Ω/12 W load resistor | * 2 Ω/12 W load resistor | ||
- | * PC (Windows 7) with USB interface | + | * // |
+ | * Windows XP up to Windows 7 OS | ||
+ | * with USB interface | ||
- | ---- | ||
===== General Setup ===== | ===== General Setup ===== | ||
==== Block Assignments ==== | ==== Block Assignments ==== | ||
- | {{ : | + | {{ : |
- Connect | - Connect | ||
- Connect a 6V power supply to the **+6V** and **GND** pins on the board. If available, a 6 V wall wart can be connected to the barrel connector, **J5**, in place of the 6V power supply. | - Connect a 6V power supply to the **+6V** and **GND** pins on the board. If available, a 6 V wall wart can be connected to the barrel connector, **J5**, in place of the 6V power supply. | ||
- Connect the 5V/2.5 A dc supply to +VIN and GND on **J1**. Also connect the 2 Ω/12 W load resistor to LOAD and GND on **J1**. | - Connect the 5V/2.5 A dc supply to +VIN and GND on **J1**. Also connect the 2 Ω/12 W load resistor to LOAD and GND on **J1**. | ||
- | {{ : | + | - **J2** is for SPI breakout. |
+ | {{ : | ||
- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
Line 40: | Line 45: | ||
- Click **Finish** to complete the installation\\ {{ : | - Click **Finish** to complete the installation\\ {{ : | ||
- | ---- | + | |
+ | |||
+ | |||
+ | ===== Running the System ===== | ||
+ | |||
+ | | ||
+ | | ||
+ | | ||
+ | - Click **“Connect”** to start communication between SDP-B and [[ADI> | ||
+ | - Upon successful connection, select SDP connector A | ||
+ | - Set the desired number of samples. | ||
+ | - Turn the 5 V/2.5 A dc supply on when data is ready to be acquired. | ||
+ | - Adjust the voltage output accordingly to output the amount of current needed to be measured | ||
+ | - Click **“Sample Data”** to start acquisition of data. | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Main Window ==== | ==== Main Window ==== | ||
- | {{ : | + | {{ : |
- | - **Title Bar** | + | - **Connect** Button - Starts the connection between the [[ADI> |
- | * **Connect** Button - Starts the connection between the [[ADI> | + | |
- | | + | - **Select SDP connector** - Selects which 120-pin connection of the SDP-B Board to use. |
- | - **Menu Bar** | + | |
- | * **Select SDP connector** - Selects which 120-pin connection of the SDP-B Board to use. | + | |
- | | + | |
- | | + | - **Sample Data** Tab\\ {{ : |
- | | + | |
- | - **Selection Tab** | + | |
- | * **Sample Data** Tab\\ | + | |
* Shows the acquired measurement data in terms of ADC codes with respect to the samples. | * Shows the acquired measurement data in terms of ADC codes with respect to the samples. | ||
* By right-clicking within the area, more functions can be viewed. Graph palette can be hidden by deselecting it and also other items can be added such as plot legend, scale legend, etc. | * By right-clicking within the area, more functions can be viewed. Graph palette can be hidden by deselecting it and also other items can be added such as plot legend, scale legend, etc. | ||
- | * **Histogram** Tab\\ | + | - **Histogram** Tab\\ {{ : |
* Shows the acquired measurement data in terms of Number of counts with respect to the ADC codes | * Shows the acquired measurement data in terms of Number of counts with respect to the ADC codes | ||
* The same as the previous tab, by right-clicking within the area, more functions can be viewed. Other items can be added such as plot legend, scale legend, etc. | * The same as the previous tab, by right-clicking within the area, more functions can be viewed. Other items can be added such as plot legend, scale legend, etc. | ||
- | * **Configure** Tab\\ | + | - **Configure** Tab\\ {{ : |
* **AD7920 Mode** - Can choose between two modes: | * **AD7920 Mode** - Can choose between two modes: | ||
* **Power Down Between Conversions** | * **Power Down Between Conversions** | ||
Line 69: | Line 84: | ||
* Closes the evaluation software. | * Closes the evaluation software. | ||
- | ---- | + | ===== Schematic, PCB Layout, Bill of Materials ===== |
- | ===== Running the System ===== | + | <WRAP round 80% download> |
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
- | - Apply power to the 6V supply (or wall wart) connected to the CN0241 evaluation board. | + | =====Registration===== |
- | - Connect USB cable from PC to the USB miniconnector on the SDP-B board. | + | <WRAP round tip 80% > |
- | - Launch **CN0241 Evaluation Software** from the default installation location. | + | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. |
- | - Click **“Connect”** to start communication between SDP-B and CN0241. | + | |
- | - Upon successful connection, select SDP connector used, either connector A or connector B. | + | |
- | - Set the desired number of samples. | + | |
- | - Turn the 5 V/2.5 A dc supply on when data is ready to be acquired. | + | |
- | | + | |
- | | + | |
+ | // End of document // | ||