resources:eval:user-guides:circuits-from-the-lab:cn0235 [03 Jan 2021 21:56]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0235 [30 Jul 2021 07:24]
Victor Calinao, Jr
Line 75: Line 75:
 \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0235:​cn0235_hardware.jpg |}} \\ \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0235:​cn0235_hardware.jpg |}} \\
   ***Step 1**. Connect the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] to [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|EVAL-SDP-CB1Z]](SDP Board) through the 120-pin SMD connector. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.\\ \\    ***Step 1**. Connect the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] to [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|EVAL-SDP-CB1Z]](SDP Board) through the 120-pin SMD connector. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.\\ \\ 
-  ***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[https://​wiki.analog.com/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​jumper_configuration|Jumper Configuration section]].\\ \\ +  ***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​jumper_configuration|Jumper Configuration section]].\\ \\ 
   ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|SDP Board]] and leave the other side of the cable(USB Type A) floated.\\ \\    ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|SDP Board]] and leave the other side of the cable(USB Type A) floated.\\ \\ 
-  ***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[https://​wiki.analog.com/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​general_setup|General Setup section]].\\ \\ +  ***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​general_setup|General Setup section]].\\ \\ 
   ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] .\\ \\    ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] .\\ \\ 
   ***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\    ***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\ 
Line 308: Line 308:
 </​WRAP>​ </​WRAP>​
  
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0235-SDPZ?&​v=Rev A|Register]] to receive all these great benefits and more!</​WRAP>​
 +
 +// End of document
resources/eval/user-guides/circuits-from-the-lab/cn0235.txt · Last modified: 30 Jul 2021 07:24 by Victor Calinao, Jr