Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0235 [03 Jan 2021 21:56]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0235 [14 Jan 2021 05:12]
Robin Getz user interwiki links
Line 75: Line 75:
 \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0235:​cn0235_hardware.jpg |}} \\ \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0235:​cn0235_hardware.jpg |}} \\
   ***Step 1**. Connect the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] to [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|EVAL-SDP-CB1Z]](SDP Board) through the 120-pin SMD connector. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.\\ \\    ***Step 1**. Connect the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] to [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|EVAL-SDP-CB1Z]](SDP Board) through the 120-pin SMD connector. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors.\\ \\ 
-  ***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[https://​wiki.analog.com/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​jumper_configuration|Jumper Configuration section]].\\ \\ +  ***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​jumper_configuration|Jumper Configuration section]].\\ \\ 
   ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|SDP Board]] and leave the other side of the cable(USB Type A) floated.\\ \\    ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[adi>​en/​system-demonstration-platform/​evaluation/​index.html|SDP Board]] and leave the other side of the cable(USB Type A) floated.\\ \\ 
-  ***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[https://​wiki.analog.com/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​general_setup|General Setup section]].\\ \\ +  ***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[/​resources/​eval/​user-guides/​circuits-from-the-lab/​cn0179#​general_setup|General Setup section]].\\ \\ 
   ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] .\\ \\    ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[adi>​EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] .\\ \\ 
   ***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\    ***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\ 
resources/eval/user-guides/circuits-from-the-lab/cn0235.txt · Last modified: 30 Jul 2021 07:24 by Victor Calinao, Jr