This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0235 [06 Dec 2017 08:39] – Added general setup and hardware description Dann Kristofer Bautista | resources:eval:user-guides:circuits-from-the-lab:cn0235 [03 Jan 2021 21:56] – fix links Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== EVAL-CN0235-EB1Z Overview ====== | ====== EVAL-CN0235-EB1Z Overview ====== | ||
- | [[http:// | + | [[adi>CN0235|CN0235]] is a Fully Isolated Lithium Ion Battery Monitoring System. Lithium ion (Li-Ion) battery stacks contain a large number of individual cells that must be monitored correctly in order to enhance the battery efficiency, prolong the battery life, and ensure safety. |
\\ | \\ | ||
\\ | \\ | ||
- | The 6-channel [[http:// | + | The 6-channel [[adi>ad7280A|AD7280A]] devices act as the primary monitor providing accurate voltage measurement data to the System Demonstration Platform (SDP-B) evaluation board, and the 6-channel [[adi>AD8280|AD8280]] devices act as the secondary monitor and protection system. Both devices can operate from a single wide supply range of 8V to 30 V and operate over the industrial temperature range of −40°C to +105°C |
\\ | \\ | ||
\\ | \\ | ||
- | The [[http:// | + | The [[adi>ad7280A|AD7280A]]contains an internal ±3 ppm reference that allows a cell voltage measurement accuracy of ±1.6 mV. The ADC resolution is 12 bits and allows conversion of up to 48 cells within 7 μs. It also has cell balancing interface outputs designed to control external FET transistors to allow discharging of individual cells and forcing all the cells in the stack to have identical voltages. |
\\ | \\ | ||
\\ | \\ | ||
- | The [[http:// | + | The [[adi>AD8280|AD8280]] functions independently of the primary monitor and provides alarm functions indicating out of tolerance conditions. It contains its own reference and LDO, both of which are powered completely from the battery cell stack. The reference, in conjunction with external resistor dividers, is used to establish trip points for the over/ |
---- | ---- | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] Evaluation Board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 31: | Line 31: | ||
---- | ---- | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>CN0235|EVAL-CN0235-SDPZ]] **(CN0235 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B board)** |
- | * The [[http:// | + | * The [[adi>CN0235|EVAL-CN0235-SDPZ]] **(CN0235 Board)** is powered by a +6V Wall wart via the DC barrel jack. |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B board)** connects to the PC via the USB-cable. |
{{ : | {{ : | ||
Line 74: | Line 74: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
\\ {{ : | \\ {{ : | ||
- | ***Step 1**. Connect the [[http:// | + | ***Step 1**. Connect the [[adi>EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] to [[adi>en/ |
***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[https:// | ***Step 2**. Do the jumper setting correctly based on desired setting for evaluation based on the jumper configuration provided on [[https:// | ||
- | ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[http:// | + | ***Step 3**. Plug the mini-USB side of the cable into the mini-USB connector J1 on [[adi>en/ |
***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[https:// | ***Step 4**. Connect the battery stack on J1 and J2 based on the number of cells configured by the jumper SEL0 and SEL1. Refer to the jumper configuration on [[https:// | ||
- | ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[http:// | + | ***Step 5**. Plug in the wallwart and connect it to the barrel jack connector of the [[adi>EVAL-CN0235-SDPZ|EVAL-CN0235-SDPZ]] .\\ \\ |
***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\ | ***Step 6**. Connect the USB-Type-A side of the USB cable to the PC.\\ \\ | ||
Line 89: | Line 89: | ||
- **Connect to SDP-B Board Button** | - **Connect to SDP-B Board Button** | ||
- | * When this button is pressed, the SDP-B Board makes a USB connection to the [[http:// | + | * When this button is pressed, the SDP-B Board makes a USB connection to the [[adi>EVAL-CN0235-SDPZ|CN0235]]Board. A connection to the SDP-B Board must be made to use the software. |
- **Device Selector** | - **Device Selector** | ||
* Selects the number of device to be activated. | * Selects the number of device to be activated. | ||
Line 99: | Line 99: | ||
* When this button is clicked, all the configuration changes on the evaluation software will be revert back to its default state. | * When this button is clicked, all the configuration changes on the evaluation software will be revert back to its default state. | ||
- **Hardware PD** | - **Hardware PD** | ||
- | * Clicking this button will put [[http:// | + | * Clicking this button will put [[adi>ad7280A|AD7280A]] in to Full Power-Down mode, meaning, both the analog and digital circuitry of the [[adi>ad7280A|AD7280A]] will be shut down, this in turn will only require 5uA maximum current. This button will also disable [[adi>AD8280|AD8280]]. |
- **Software PD** | - **Software PD** | ||
- | * . Clicking this button will put [[http:// | + | * . Clicking this button will put [[adi>ad7280A|AD7280A]] in to Software Power-Down mode which requires only 3.8 mA maximum current. This button will also disable [[adi>AD8280|AD8280]]. |
- **Software/ | - **Software/ | ||
- | *Clicking this button will power up the [[http:// | + | *Clicking this button will power up the [[adi>ad7280A|AD7280A]] when it’s coming from a software power down or hardware power down mode. This button will not enable the [[adi>AD8280|AD8280]]. |
- **Enable/ | - **Enable/ | ||
* This button allows the user to enable or disable the secondary battery monitoring and protection system. | * This button allows the user to enable or disable the secondary battery monitoring and protection system. | ||
Line 265: | Line 265: | ||
* Sets the on-time of each Cell Balance output. The timer may be set from 0 minutes to 36.9 minutes with a 71.5second resolution. See {{http:// | * Sets the on-time of each Cell Balance output. The timer may be set from 0 minutes to 36.9 minutes with a 71.5second resolution. See {{http:// | ||
- **Thermistor Term Resistor** | - **Thermistor Term Resistor** | ||
- | * Sets if the thermistor termination pin //AUXterm// will be used to terminate the thermistor inputs for each auxiliary ADC input of the AD7280A. \\ <WRAP round info 65%> | + | * Sets if the thermistor termination pin //AUXterm// will be used to terminate the thermistor inputs for each auxiliary ADC input of the AD7280A. \\ <WRAP round info 65%> |
Line 275: | Line 275: | ||
\\ | \\ | ||
\\ | \\ | ||
- | The advanced tab allows the user to read/write to the [[http:// | + | The advanced tab allows the user to read/write to the [[adi>ad7280A|AD7280A]]’s registers. |
\\ | \\ | ||
- | <WRAP left tip round box 60%> | + | <WRAP left tip round box 60%> |
\\ \\ \\ \\ \\ \\ \\ | \\ \\ \\ \\ \\ \\ \\ | ||
- **Dev0 and Dev1 Register Address** | - **Dev0 and Dev1 Register Address** | ||
- | * This the list of the register address of [[http:// | + | * This the list of the register address of [[adi>ad7280A|AD7280A]] and its current content or configuration. |
- **Read Register** | - **Read Register** | ||
* This button updates the register address array of both devices. | * This button updates the register address array of both devices. | ||
- **Write Register** | - **Write Register** | ||
- | * Use this function to write a new value to a certain register of [[http:// | + | * Use this function to write a new value to a certain register of [[adi>ad7280A|AD7280A]]. |
\\ | \\ | ||
Line 301: | Line 301: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>CN0235-DesignSupport|EVAL-CN0235-SDPZ Design & Integration Files]] |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout |