This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0233 [05 May 2015 19:52] – formatting Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0233 [24 Apr 2024 07:34] (current) – added deprecated note Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======CN-0233 Software | + | ====== |
+ | |||
+ | <WRAP round important 65%> | ||
+ | \\ | ||
+ | This reference design has been **RETIRED** or **DEPRECATED**, | ||
+ | \\ | ||
+ | This page is here for historical/ | ||
+ | \\ | ||
+ | </ | ||
===== OVERVIEW ===== | ===== OVERVIEW ===== | ||
Line 9: | Line 18: | ||
===== GENERAL SETUP ===== | ===== GENERAL SETUP ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0233-SDPZ|EVAL-CN0233-SDPZ]] Evaluation Board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 41: | Line 50: | ||
===== STEP BY STEP INSTRUCTION FOR CONNECTING THE HARDWARE ===== | ===== STEP BY STEP INSTRUCTION FOR CONNECTING THE HARDWARE ===== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[http:// | + | - Connect the 120-pin connector on the [[adi>EVAL-CN0233-SDPZ|EVAL-CN0233-SDPZ]] circuit board to the connector marked “CON A” on the EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors as depicted in the image below. |
- | - Connect a voltmeter to Vout of [[http:// | + | - Connect a voltmeter to Vout of [[adi>EVAL-CN0233-SDPZ|EVAL-CN0233-SDPZ]]. |
- | - Connect a current meter to Iout of [[http:// | + | - Connect a current meter to Iout of [[adi>EVAL-CN0233-SDPZ|EVAL-CN0233-SDPZ]]. |
- | - To power on the [[http:// | + | - To power on the [[adi>EVAL-CN0233-SDPZ|EVAL-CN0233-SDPZ]], |
- | - Connect the USB cable, supplied along with the [[http:// | + | - Connect the USB cable, supplied along with the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation board, from the SDP board to the USB port on the PC. |
---- | ---- | ||
Line 84: | Line 93: | ||
- SDP Board Firmware Revision – provides details on the firmware version of the Blackfin used by the SDP board. | - SDP Board Firmware Revision – provides details on the firmware version of the Blackfin used by the SDP board. | ||
+ | \\ | ||
+ | \\ | ||
+ | // End of document // | ||