This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0229 [07 Aug 2017 05:55] – created Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0229 [30 Jul 2021 07:23] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 3: | Line 3: | ||
[[ADI> | [[ADI> | ||
- | The [[ADI>AD5750/ | + | The [[ADI> |
The [[ADI> | The [[ADI> | ||
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Triple Output DC Power Supply (6 V, +15 V and -15 V) | * Triple Output DC Power Supply (6 V, +15 V and -15 V) | ||
Line 22: | Line 22: | ||
* //Agilent 34401A 6.5 Digital Multimeter// | * //Agilent 34401A 6.5 Digital Multimeter// | ||
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
- | * Windows | + | * Windows |
* USB interface | * USB interface | ||
- | * USB type A to USB type mini-B cable | ||
---- | ---- | ||
===== General Setup ===== | ===== General Setup ===== | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
- | {{ : | + | {{ : |
- | * The [[http:// | + | * The [[adi>EVAL-CN0229-SDPZ|EVAL-CN0229-SDPZ]] **(CN-0229 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * Terminal block CN1 is the +/- 15 V power supply input | + | * Terminal block **CN1** is the +/- 15 V power supply input |
- | * Terminal block CN2 is the +6 V power supply input | + | * Terminal block **CN2** is the +6 V power supply input |
- | * 4 channels | + | * Four OUT_[x] voltage/ |
+ | * **Optionally**, | ||
\\ | \\ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Do not connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the EVAL-CN0229-SDPZ. | + | |
</ | </ | ||
==== Jumper settings ==== | ==== Jumper settings ==== | ||
See image below for jumper settings. The bolded values are the default settings for the EVAL-CN0229-SPDZ. | See image below for jumper settings. The bolded values are the default settings for the EVAL-CN0229-SPDZ. | ||
- | {{ : | + | |
+ | {{ : | ||
---- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
Line 55: | Line 56: | ||
---- | ---- | ||
+ | ===== Using the Evaluation Software ===== | ||
+ | ====Main Tab==== | ||
+ | {{ : | ||
+ | * **Connection** <fc # | ||
+ | * **Connect Button** | ||
+ | * Starts the connection with the [[ADI> | ||
+ | * **Disconnect Button** | ||
+ | * Ends the connection with the [[ADI> | ||
+ | |||
+ | * **System Configuration** <fc # | ||
+ | * **Connector** | ||
+ | * Selects which 120-pin connection of the SDP-B Board to use | ||
+ | * **SLCK** | ||
+ | * Sets the SPI clock frequency used by the evaluation board | ||
+ | |||
+ | * **Set/ | ||
+ | * **Reset** | ||
+ | * Resets AD5686R | ||
+ | * **Set All** | ||
+ | * Sets all channels to their corresponding settings | ||
+ | * **Quit** | ||
+ | * Exit the application | ||
+ | |||
+ | |||
+ | * **Channel 1 Settings** <fc # | ||
+ | * **Output** | ||
+ | * Enables or disables Channel 1 | ||
+ | * **Range** | ||
+ | * Sets the voltage/ | ||
+ | * **Value** | ||
+ | * Sets the hex value corresponding to the desired output level in Channel 1 | ||
+ | |||
+ | * **Channel 2 Settings** <fc # | ||
+ | * **Output** | ||
+ | * Enables or disables Channel 2 | ||
+ | * **Range** | ||
+ | * Sets the voltage/ | ||
+ | * **Value** | ||
+ | * Sets the hex value corresponding to the desired output level in Channel 2 | ||
+ | |||
+ | * **Channel 3 Settings** <fc # | ||
+ | * **Output** | ||
+ | * Enables or disables Channel 3 | ||
+ | * **Range** | ||
+ | * Sets the voltage/ | ||
+ | * **Value** | ||
+ | * Sets the hex value corresponding to the desired output level in Channel 3 | ||
+ | |||
+ | * **Channel 4 Settings** <fc # | ||
+ | * **Output** | ||
+ | * Enables or disables Channel 4 | ||
+ | * **Range** | ||
+ | * Sets the voltage/ | ||
+ | * **Value** | ||
+ | * Sets the hex value corresponding to the desired output level in Channel 4 | ||
+ | |||
+ | \\ | ||
+ | ==== Running the System ==== | ||
+ | - Open the **CN0229.exe** application from the default installation location. | ||
+ | - Set the correct connector and SCLK settings for the board in the System Configuration section. | ||
+ | - Click the **Connect Button** | ||
+ | - Upon successful connection, select the desired channel to be used. | ||
+ | - Set the output of the channel to enable. | ||
+ | - Select the range of desired output. | ||
+ | - Input a corresponding hex value of the output level and select **Set CH[x]**. | ||
+ | - In case all channels are to be used, set all desired settings for each channel and click the **Set ALL button**. | ||
+ | - Click **Disconnect Button** if finished. | ||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== More Information and Useful Links ===== | ||
+ | * [[ftp:// | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | //End of Document// | ||
+ |