Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0225 [02 Nov 2017 05:08] Angelo Nikko Catapangresources:eval:user-guides:circuits-from-the-lab:cn0225 [30 Jul 2021 07:23] (current) Victor Calinao, Jr
Line 26: Line 26:
 ===== General Setup ===== ===== General Setup =====
 ==== Block Assignments ==== ==== Block Assignments ====
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0225:cn0225-hw-1024-edited.jpg?nolink&600 |}}+{{:resources:eval:user-guides:circuits-from-the-lab:cn0225:cn0225-hw-1024-edited.jpg?nolink&600|}}
   * The [[ADI>CN0225|EVAL-CN0225-SDPZ]] **(CN0225 Board)** connects to the [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin Connector **(SDP Conn)**   * The [[ADI>CN0225|EVAL-CN0225-SDPZ]] **(CN0225 Board)** connects to the [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin Connector **(SDP Conn)**
   * The [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable   * The [[ADI>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable
Line 33: Line 33:
   * Terminal block **J3** is the +/- 15 V power supply input   * Terminal block **J3** is the +/- 15 V power supply input
   * Terminal block **J4** contains the test points for the SPI signals   * Terminal block **J4** contains the test points for the SPI signals
-<WRAP center round important 60%>Power on the **(EVAL-CN0225-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</WRAP>+<WRAP center round important 60%>Connect the **(EVAL-CN0225-SDPZ)** and the **(SDP-B Board)**, then power the **(EVAL-CN0225-SDPZ)** through the triple output power supply before connecting the **(SDP-B Board)** to the PC</WRAP> 
 + 
 +==== Setup Block Diagram ==== 
 + 
 +{{:resources:eval:user-guides:circuits-from-the-lab:cn0225:cn0225-03-1024.png?nolink&600|}} 
 + 
 +==== Jumper Settings ==== 
 +See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>CN0225|EVAL-CN0225-SDPZ]] 
 + 
 +{{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-45-44_pm.png?nolink&600|}} 
 + 
 +---- 
 + 
 +===== Installing the Evaluation Software ===== 
 +  - Extract the file **[[ftp://ftp.analog.com/pub/cftl/CN0225/CN0225%20SDP%20Eval%20Software.zip|CN0225 Evaluation Software]]** and open **setup.exe**\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0203/CN0203%20SDP%20Eval%20Software.zip|CN0203 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-51-12_pm.png?nolink&600|}} 
 +  - Press **Next** to view the National Instruments Software License Agreement\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-52-02_pm.png?nolink&600|}} 
 +  - Select the option which **accepts** the License Agreement and press **Next** to view the installation review page\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-52-35_pm.png?nolink&600|}} 
 +  - Press **Next** to start the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-53-43_pm.png?nolink&600|}} 
 +  - Upon completion of the installation of the **CN0225 Evaluation Software**, the installer for the ADI SDP Drivers will execute\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-55-25_pm.png?nolink&600 |}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-55-36_pm.png?nolink&600|}} 
 +  - Press **“Next”** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-54-25_pm.png?nolink&600|}} 
 +  - Press **“Next”** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-55-25_pm.png?nolink&600|}} 
 +  - Press **Finish** to complete the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-55-36_pm.png?nolink&600|}} 
 +  - **(Optional)** Restart the PC when prompted by the installer\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0225:11-2-2017_3-56-02_pm.png?nolink&600|}} 
 + 
 +---- 
 +===== Using the Evaluation Software ===== 
 +==== Main Window ==== 
 +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0225:11-3-2017_3-29-38_pm_-_edited.png?nolink&600 |}} 
 +  - **Board Connection Control Section** 
 +      * **Connect Button** 
 +          * Starts the connection with the [[ADI>CN0225|CN0225 Evaluation Board]] 
 +      * **Disconnect Button** 
 +          * Ends the connection with the [[ADI>CN0225|CN0225 Evaluation Board]] 
 +      * **STOP APP Button** 
 +          * Exits the software application 
 +  - **Data Acquisition Control Section** 
 +      * **connector Select** 
 +          * Selects which 120-pin connection of the **SDP-B Board** to use 
 +      * **Fs (Hz) Field** 
 +          * Sets the sampling frequency of the CN0225 ADC 
 +      * **Samples Field** 
 +          * Sets the number of samples the CN0225 ADC takes 
 +      * **SCLK (Hz) Field** 
 +          * Sets the SPI clock frequency used by the evaluation board 
 +      * **Acquire Samples Button** 
 +          * Commands the **CN0225** ADC to sample at the set sampling frequency and read the set number of samples 
 +      * **Save Data to File Button** 
 +          * Saves the current sample readings to an output file 
 +  - **Activity Frame** 
 +      * **Time Domain Tab** 
 +          * Displays the measured ADC sample values vs time plot 
 +      * **Frequency Domain Tab** 
 +          * Plots the FFT of the the ADC samples with the amplitudse in dB of the full scale ADC value 
 +            {{ :resources:eval:user-guides:circuits-from-the-lab:cn0225:11-3-2017_3-30-08_pm_-_edited.png?nolink&600 |}} 
 +      * **Histogram** 
 +          * Plots the number of occurrences of ADC sample values 
 +            {{ :resources:eval:user-guides:circuits-from-the-lab:cn0225:11-3-2017_3-30-27_pm_-_edited.png?nolink&600 |}} 
 +      * **S/W Version Info** 
 +          * Shows the software and hardware versions, vendor and product IDs 
 +          * **Flash LED Button** tests the SDP communication to the **CN0225** 
 +          * **Read Firmware Button** reads the current SDP firmware for debugging 
 +            {{ :resources:eval:user-guides:circuits-from-the-lab:cn0225:11-3-2017_3-30-38_pm_-_edited.png?nolink&600 |}} 
 +==== Running the System ==== 
 +  - Open the **CN0225.exe** application from the default installation location. 
 +  - Set the correct connector and SCLK settings for the board in the **Data Acquisition Control** 
 +  - Click the **Connect Button** 
 +  - Set the desired sampling frequency in Hz and the number of samples to read 
 +  - Click **Acquire Samples Button** 
 +  - Click the **Time Domain Tab** to view the ADC sample values vs time plot 
 +  - Click the **Frequency Domain Tab** to view the FFT plot of the sample values 
 +  - Click the **Histogram Tab** to view the number of occurrences of ADC sample values 
 +  - Click the **S/W Version Info Tab** to view the hardware and software versions 
 +  - Click **Save Data to File Button** if you want to save the current sample readings 
 +  - Click the **Disconnect Button** if finished 
 +  - Click the **STOP APP Button** to exit the software 
 + 
 +---- 
 + 
 +===== More Information and Useful Links ===== 
 +  * [[ftp://ftp.analog.com/pub/cftl/CN0225/CN0225%20SDP%20Eval%20Software.zip|CN0225 Evaluation Software]] 
 +  * [[ADI>CN0225|CN0225 Circuit Note Page]] 
 +  * [[ADI>CN0225 -DesignSupport|CN0225 Design Support Package]] 
 +  * [[ADI>AD7687|AD7687 Product Page]] 
 +  * [[ADI>AD8275|AD8275 Product Page]] 
 +  * [[ADI>AD8295|AD8295 Product Page]] 
 +  * [[ADI>ADR431|ADR431 Product Page]] 
 + 
 +===== Schematic, PCB Layout, Bill of Materials ===== 
 + 
 +<WRAP round 80% download> 
 +[[adi>media/en/reference-design-documentation/design-integration-files/CN02225-DesignSupport.zip|EVAL-CN0225-SDPZ Design & Integration Files]] 
 +  * Schematics  
 +  * PCB Layout  
 +  * Bill of Materials  
 +  * PADS project 
 +</WRAP> 
 + 
 +=====Registration=====  
 +<WRAP round tip 80% > 
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0225-SDPZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP> 
 + 
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0225.1509595715.txt.gz · Last modified: 02 Nov 2017 05:08 by Angelo Nikko Catapang