Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0204 [07 Aug 2017 08:36]
ACatapang
resources:eval:user-guides:circuits-from-the-lab:cn0204 [21 Sep 2017 18:51] (current)
Brandon adding design files
Line 21: Line 21:
   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)
   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)
-  * PC (Windows 2000 or Windows XP) with USB interface+  * PC with USB interface 
 +      * Windows 7 or higher
  
 ---- ----
Line 36: Line 37:
       * Connect the **-25 V** power supply to the **GND_ISO** terminal       * Connect the **-25 V** power supply to the **GND_ISO** terminal
   * Terminal block **CN4** is the voltage output   * Terminal block **CN4** is the voltage output
-      * **Optionally**,​ the [[ADI>​AD5751]] ​output voltage feedback can be configured by connecting **VSENSE+** to a selected node in the load circuit+      * **Optionally** ​if **JP3** is open, the output voltage feedback can be configured by connecting **VSENSE+** to a selected node in the load circuit
 <WRAP center round important 60%>​Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</​WRAP>​ <WRAP center round important 60%>​Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</​WRAP>​
  
 ==== Jumper Settings ==== ==== Jumper Settings ====
-See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]].+See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]].
  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2.jpg?​nolink&​600 |}}+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_5.jpg?​nolink&​600 |}}
  
 ---- ----
Line 110: Line 111:
   * [[ADI>​AD5662|AD5662 Product Page]]   * [[ADI>​AD5662|AD5662 Product Page]]
   * [[ADI>​AD5751|AD5751 Product Page]]   * [[ADI>​AD5751|AD5751 Product Page]]
 +
 +
 +===== Schematic, PCB Layout, Bill of Materials =====
 +
 +<WRAP round 80% download>​
 +[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0204-DesignSupport.zip|EVAL-CN0204-SDPZ Design & Integration Files]]
 +  * Schematics ​
 +  * PCB Layout ​
 +  * Bill of Materials ​
 +  * PADS project
 +</​WRAP>​
 +
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0204.1502087777.txt.gz · Last modified: 07 Aug 2017 08:36 by ACatapang