Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0204 [04 Aug 2017 08:58]
ACatapang
resources:eval:user-guides:circuits-from-the-lab:cn0204 [21 Sep 2017 18:51] (current)
Brandon adding design files
Line 21: Line 21:
   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)
   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)
-  * PC (Windows 2000 or Windows XP) with USB interface+  * PC with USB interface 
 +      * Windows 7 or higher
  
 ---- ----
Line 36: Line 37:
       * Connect the **-25 V** power supply to the **GND_ISO** terminal       * Connect the **-25 V** power supply to the **GND_ISO** terminal
   * Terminal block **CN4** is the voltage output   * Terminal block **CN4** is the voltage output
-      * **Optionally**,​ the [[ADI>​5751]] ​output voltage feedback can be configured by connecting VSENSE+ to a selected node in the load circuit+      * **Optionally** ​if **JP3** is open, the output voltage feedback can be configured by connecting ​**VSENSE+** to a selected node in the load circuit
 <WRAP center round important 60%>​Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</​WRAP>​ <WRAP center round important 60%>​Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</​WRAP>​
  
 ==== Jumper Settings ==== ==== Jumper Settings ====
-See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI>CN0203|EVAL-CN0203-SDPZ]].+See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>CN0204|EVAL-CN0204-SDPZ]].
  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2.jpg?​nolink&​600 |}}+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_5.jpg?​nolink&​600 |}}
  
 ---- ----
  
 ===== Installing the Evaluation Software ===== ===== Installing the Evaluation Software =====
-  - Ordered List Item+  - Extract the file **[[ftp://​ftp.analog.com/​pub/​cftl/​CN0204/​CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]]** and open **setup.exe**\\ <WRAP left tip round box 60%>​**NOTE:​** It is recommended that you install the [[ftp://​ftp.analog.com/​pub/​cftl/​CN0204/​CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]] to the default directory path **C:​\Program Files (x86)\Analog Devices\CN0204\** and all National Instruments products to **C:​\Program Files\National Instruments\**</​WRAP>​\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-19-32_am.png?​nolink&​600|}} 
 +  - Press **Next** to view the installation review page\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-19-42_am.png?​nolink&​600|}} 
 +  - Press **Next** to start the installation\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-20-11_am.png?​nolink&​600|}} 
 +  - Upon completion of the installation of the **CN0204 Evaluation Software**, the installer for the ADI SDP Drivers will execute.\\ <WRAP left tip round box 60%>​**NOTE:​** It is recommended that you close all other applications before clicking **“Next”**. ​ This will make it possible to update relevant system files without having to reboot your computer.</​WRAP>​\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-20-38_am.png?​nolink&​600|}} 
 +  - Press **Next** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:​\Program Files\Analog Devices\SDP\Drivers**</​WRAP>​\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-20-47_am.png?​nolink&​600|}} 
 +  - Press **Next** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​7-27-2017_10-22-01_am.png?​nolink&​600|}} 
 +  - Press **Finish** to complete the installation\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​8-1-2017_10-21-55_am.png?​nolink&​600|}} 
 + 
 +---- 
 + 
 +===== Using the Evaluation Software ===== 
 +==== Main Window ==== 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​7-27-2017_10-29-07_am_-_edit.jpg?​nolink&​600 |}} 
 +  * **Title Bar** <fc #​9400d3>​(Highlighted Violet)</​fc>​ 
 +      * **Connect Button** 
 +          * Starts the connection with the [[ADI>​CN0204|CN0204 Evaluation Board]] 
 +      * **Disconnect Button** 
 +          * Ends the connection with the [[ADI>​CN0204|CN0204 Evaluation Board]] 
 +  * **System Configuration** <fc #​ffa500>​(Highlighted Orange)</​fc>​ 
 +      * **Connector** 
 +          * Selects which 120-pin connection of the **SDP-B Board** to use 
 +      * **SCLK (Hz)** 
 +          * Sets the SPI clock frequency used by the evaluation board 
 +  * **AD5751 Configuration** <fc #​4682b4>​(Highlighted Blue)</​fc>​ 
 +      * **JP1 Configuration** 
 +          * Sets the SPI address of the AD5750-1 based on the position of JP1 
 +      * **Range Select** 
 +          * Sets the voltage/​current output range 
 +      * **Toggle CLEAR** 
 +          * Sets the outputs to the zero/​midscale voltage value or the minimum value of the selected current range 
 +  * **AD5751 Error Indicator** <fc #​ffff00>​(Highlighted Yellow)</​fc>​ 
 +      * **Vout Fault** 
 +          * There is a short circuit on the VOUT pin 
 +      * **Iout Fault** 
 +          * There is an open circuit on the IOUT pin 
 +      * **Over Temp** 
 +          * The AD5751 core temperature exceeds 150 °C 
 +      * **PEC Error** 
 +          * CRC-8 error checking detected an interface error 
 +  * **Output Setting** <fc #​ff0000>​Highlighted Red</​fc>​ 
 +      * **Write AD5662** 
 +          * Writes the hexadecimal value in the left field to the AD5662 output voltage 
 +      * **Reset AD5751** 
 +          * Resets the AD5751 to its power-on state 
 +  * **Quit** 
 +      * Exits the software application 
 +==== Running the System ==== 
 +  - Open the **CN0204.exe** application from the default installation location. 
 +  - Set the correct connector and SCLK settings for the board in the System Configuration section. 
 +  - Click the **Connect Button**  
 +  - Upon successful connection, select the desired range of output on the Range Select drop-down menu. 
 +  - Input a hex value equivalent of the desired output level in the Output Setting section. 
 +  - Click **Write AD5662** 
 +  - Click **Disconnect Button** if finished. 
 + 
 +---- 
 + 
 +===== More Information and Useful Links ===== 
 +  * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0204/​CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]] 
 +  * [[ADI>​CN0204|CN0204 Circuit Note Page]] 
 +  * [[ADI>​CN0204 -DesignSupport|CN0204 Design Support Package]] 
 +  * [[ADI>​AD5662|AD5662 Product Page]] 
 +  * [[ADI>​AD5751|AD5751 Product Page]] 
 + 
 + 
 +===== Schematic, PCB Layout, Bill of Materials ===== 
 + 
 +<WRAP round 80% download>​ 
 +[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0204-DesignSupport.zip|EVAL-CN0204-SDPZ Design & Integration Files]] 
 +  * Schematics  
 +  * PCB Layout  
 +  * Bill of Materials  
 +  * PADS project 
 +</​WRAP>​ 
 + 
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0204.1501829934.txt.gz · Last modified: 04 Aug 2017 08:58 by ACatapang