Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0204 [07 Aug 2017 06:09] Angelo Nikko Catapangresources:eval:user-guides:circuits-from-the-lab:cn0204 [21 Sep 2017 18:51] – adding design files Brandon Bushey
Line 21: Line 21:
   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)
   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)
-  * PC (Windows 2000 or Windows XP) with USB interface+  * PC with USB interface 
 +      * Windows 7 or higher
  
 ---- ----
Line 36: Line 37:
       * Connect the **-25 V** power supply to the **GND_ISO** terminal       * Connect the **-25 V** power supply to the **GND_ISO** terminal
   * Terminal block **CN4** is the voltage output   * Terminal block **CN4** is the voltage output
-      * **Optionally**, the [[ADI>5751]] output voltage feedback can be configured by connecting **VSENSE+** to a selected node in the load circuit+      * **Optionally** if **JP3** is open, the output voltage feedback can be configured by connecting **VSENSE+** to a selected node in the load circuit
 <WRAP center round important 60%>Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</WRAP> <WRAP center round important 60%>Power on the **(EVAL-CN0204-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **SEPARATELY** before connecting the two boards together.</WRAP>
  
 ==== Jumper Settings ==== ==== Jumper Settings ====
-See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI>CN0204|EVAL-CN0204-SDPZ]].+See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>CN0204|EVAL-CN0204-SDPZ]].
  
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:cn0204_table2.jpg?nolink&600 |}}+{{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:cn0204_table2_5.jpg?nolink&600 |}}
  
 ---- ----
  
 ===== Installing the Evaluation Software ===== ===== Installing the Evaluation Software =====
-  - Extract the file **[[ftp://ftp.analog.com/pub/cftl/CN0204/CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]]** and open **setup.exe**\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0204/CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0204\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-19-32_am.png?nolink&600 |}} +  - Extract the file **[[ftp://ftp.analog.com/pub/cftl/CN0204/CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]]** and open **setup.exe**\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0204/CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0204\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-19-32_am.png?nolink&600|}} 
-  - Press **Next** to view the installation review page\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-19-42_am.png?nolink&600 |}} +  - Press **Next** to view the installation review page\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-19-42_am.png?nolink&600|}} 
-  - Press **Next** to start the installation\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-11_am.png?nolink&600 |}} +  - Press **Next** to start the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-11_am.png?nolink&600|}} 
-  - Upon completion of the installation of the **CN0204 Evaluation Software**, the installer for the ADI SDP Drivers will execute.\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-38_am.png?nolink&600 |}} +  - Upon completion of the installation of the **CN0204 Evaluation Software**, the installer for the ADI SDP Drivers will execute.\\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-38_am.png?nolink&600|}} 
-  - Press **Next** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-47_am.png?nolink&600 |}} +  - Press **Next** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-20-47_am.png?nolink&600|}} 
-  - Press **Next** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:7-27-2017_10-22-01_am.png?nolink&600 |}} +  - Press **Next** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:7-27-2017_10-22-01_am.png?nolink&600|}} 
-  - Press **Finish** to complete the installation\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-21-55_am.png?nolink&600 |}}+  - Press **Finish** to complete the installation\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0204:8-1-2017_10-21-55_am.png?nolink&600|}}
  
 ---- ----
Line 59: Line 60:
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ==== Main Window ==== ==== Main Window ====
 +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0204:7-27-2017_10-29-07_am_-_edit.jpg?nolink&600 |}}
 +  * **Title Bar** <fc #9400d3>(Highlighted Violet)</fc>
 +      * **Connect Button**
 +          * Starts the connection with the [[ADI>CN0204|CN0204 Evaluation Board]]
 +      * **Disconnect Button**
 +          * Ends the connection with the [[ADI>CN0204|CN0204 Evaluation Board]]
 +  * **System Configuration** <fc #ffa500>(Highlighted Orange)</fc>
 +      * **Connector**
 +          * Selects which 120-pin connection of the **SDP-B Board** to use
 +      * **SCLK (Hz)**
 +          * Sets the SPI clock frequency used by the evaluation board
 +  * **AD5751 Configuration** <fc #4682b4>(Highlighted Blue)</fc>
 +      * **JP1 Configuration**
 +          * Sets the SPI address of the AD5750-1 based on the position of JP1
 +      * **Range Select**
 +          * Sets the voltage/current output range
 +      * **Toggle CLEAR**
 +          * Sets the outputs to the zero/midscale voltage value or the minimum value of the selected current range
 +  * **AD5751 Error Indicator** <fc #ffff00>(Highlighted Yellow)</fc>
 +      * **Vout Fault**
 +          * There is a short circuit on the VOUT pin
 +      * **Iout Fault**
 +          * There is an open circuit on the IOUT pin
 +      * **Over Temp**
 +          * The AD5751 core temperature exceeds 150 °C
 +      * **PEC Error**
 +          * CRC-8 error checking detected an interface error
 +  * **Output Setting** <fc #ff0000>Highlighted Red</fc>
 +      * **Write AD5662**
 +          * Writes the hexadecimal value in the left field to the AD5662 output voltage
 +      * **Reset AD5751**
 +          * Resets the AD5751 to its power-on state
 +  * **Quit**
 +      * Exits the software application
 +==== Running the System ====
 +  - Open the **CN0204.exe** application from the default installation location.
 +  - Set the correct connector and SCLK settings for the board in the System Configuration section.
 +  - Click the **Connect Button** 
 +  - Upon successful connection, select the desired range of output on the Range Select drop-down menu.
 +  - Input a hex value equivalent of the desired output level in the Output Setting section.
 +  - Click **Write AD5662**
 +  - Click **Disconnect Button** if finished.
  
 +----
 +
 +===== More Information and Useful Links =====
 +  * [[ftp://ftp.analog.com/pub/cftl/CN0204/CN0204%20SDP%20Eval%20Software.zip|CN0204 Evaluation Software]]
 +  * [[ADI>CN0204|CN0204 Circuit Note Page]]
 +  * [[ADI>CN0204 -DesignSupport|CN0204 Design Support Package]]
 +  * [[ADI>AD5662|AD5662 Product Page]]
 +  * [[ADI>AD5751|AD5751 Product Page]]
 +
 +
 +===== Schematic, PCB Layout, Bill of Materials =====
 +
 +<WRAP round 80% download>
 +[[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0204-DesignSupport.zip|EVAL-CN0204-SDPZ Design & Integration Files]]
 +  * Schematics 
 +  * PCB Layout 
 +  * Bill of Materials 
 +  * PADS project
 +</WRAP>
 +
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0204.txt · Last modified: 30 Jul 2021 07:20 by Victor Calinao, Jr