Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0204 [06 Sep 2017 09:53]
ACatapang
resources:eval:user-guides:circuits-from-the-lab:cn0204 [21 Sep 2017 18:51]
Brandon adding design files
Line 21: Line 21:
   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)
   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)
-  * PC (Windows 7) with USB interface+  * PC with USB interface 
 +      * Windows 7 or higher
  
 ---- ----
Line 42: Line 43:
 See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]]. See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]].
  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_4.jpg?​nolink&​600 |}}+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_5.jpg?​nolink&​600 |}}
  
 ---- ----
Line 110: Line 111:
   * [[ADI>​AD5662|AD5662 Product Page]]   * [[ADI>​AD5662|AD5662 Product Page]]
   * [[ADI>​AD5751|AD5751 Product Page]]   * [[ADI>​AD5751|AD5751 Product Page]]
 +
 +
 +===== Schematic, PCB Layout, Bill of Materials =====
 +
 +<WRAP round 80% download>​
 +[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0204-DesignSupport.zip|EVAL-CN0204-SDPZ Design & Integration Files]]
 +  * Schematics ​
 +  * PCB Layout ​
 +  * Bill of Materials ​
 +  * PADS project
 +</​WRAP>​
 +
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0204.txt · Last modified: 21 Sep 2017 18:51 by Brandon