Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0204 [06 Sep 2017 09:49]
ACatapang
resources:eval:user-guides:circuits-from-the-lab:cn0204 [11 Sep 2017 07:56]
ACatapang
Line 21: Line 21:
   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)   * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**)
   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)   * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**)
-  * PC (Windows 7) with USB interface+  * PC with USB interface 
 +      * Windows 7 or higher
  
 ---- ----
Line 42: Line 43:
 See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]]. See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI>​CN0204|EVAL-CN0204-SDPZ]].
  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_3.jpg?​nolink&​600 |}}+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0204:​cn0204_table2_5.jpg?​nolink&​600 |}}
  
 ---- ----
resources/eval/user-guides/circuits-from-the-lab/cn0204.txt · Last modified: 21 Sep 2017 18:51 by Brandon