This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0202 [01 Aug 2017 08:56] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0202 [30 Jul 2021 07:19] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0202 Evaluation Board Guide ====== | ====== CN0202 Evaluation Board Guide ====== | ||
===== Overview ===== | ===== Overview ===== | ||
- | [[ADI>CN202]] a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, | + | [[ADI>CN0202]] is a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, |
- | The [[ADI> | + | The [[ADI> |
The [[ADI> | The [[ADI> | ||
Line 14: | Line 14: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Triple Output DC Power Supply (6 V, +15 V and -15 V) | * Triple Output DC Power Supply (6 V, +15 V and -15 V) | ||
+ | * //Agilent E3631A 0 V to 6 V/5 A; ±25 V/1 A Triple Output DC Power Supply// | ||
+ | * Digital Multimeter for Verification (**Optional**) | ||
+ | * //Agilent 34401A 6.5 Digital Multimeter// | ||
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
- | * Windows | + | * Windows |
* USB interface | * USB interface | ||
- | * USB type A to USB type mini-B cable | ||
---- | ---- | ||
Line 26: | Line 28: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ]] **(CN-0202 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * Terminal block CN1 is the +/- 15 V power supply input | + | * Terminal block **CN1** is the +/- 15 V power supply input |
- | * Terminal block CN2 is the +6 V power supply input | + | * Terminal block **CN2** is the +6 V power supply input |
- | * Terminal block CN3 is for the voltage output measurement | + | * Terminal block **CN3** is for the voltage output measurement |
- | * Terminal block CN4 is for the current output measurement | + | * **Optionally**, |
+ | * Terminal block **CN4** is for the current output measurement | ||
\\ | \\ | ||
Line 40: | Line 43: | ||
==== Jumper settings ==== | ==== Jumper settings ==== | ||
- | See image below for jumper settings. | + | See the table in the image below for the jumper settings. |
- | {{ : | + | |
+ | {{ : | ||
---- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
Line 53: | Line 58: | ||
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
- | ===Main Tab=== | + | ====Main Tab==== |
- | {{ : | + | {{ : |
- | | + | * **Connection** <fc # |
- | * Connect | + | * **Connect |
- | | + | * Starts the connection |
- | * Selects | + | * **Disconnect Button** |
- | | + | * Ends the connection with the [[ADI> |
- | * Sets the clock frequency used by the AD5750, AD5662 and SDP | + | |
- | - **JP1 Configuration** | + | |
- | * Sets the address of AD5750 | + | * **Connector** |
- | | + | * Selects |
- | * Sets the voltage/ | + | |
- | | + | * Sets the SPI clock frequency used by the evaluation board |
- | * Sets the outputs to a zero scale/midscale voltage | + | |
- | - **Write AD5662** | + | |
- | * Writes to AD5662 | + | * **JP1 Configuration** |
- | | + | * Sets the SPI address of the AD5750-1 based on the position of JP1 |
- | * Resets | + | * **Range Select** |
- | | + | * Sets the voltage/ |
- | * Displays errors in AD5750 | + | * **Toggle CLEAR** |
- | - **Disconnect** | + | * Sets the outputs to the zero/ |
- | * Stop communication with the evaluation board | + | |
- | | + | |
- | * Exit the application | + | * **Vout Fault** |
+ | * There is a short circuit on the VOUT pin | ||
+ | * **Iout Fault** | ||
+ | * There is an open circuit on the IOUT pin | ||
+ | * **Over Temp** | ||
+ | * The AD5750-1 core temperature exceeds 150 °C | ||
+ | * **PEC Error** | ||
+ | * CRC-8 error checking detected an interface error | ||
+ | |||
+ | | ||
+ | * **Write AD5660-1** | ||
+ | * Writes the hexadecimal value in the left field to the AD5660-1 output voltage | ||
+ | * **Reset AD5750-1** | ||
+ | * Resets | ||
+ | |||
+ | | ||
+ | * Exits the software | ||
\\ | \\ | ||
- | === Running the System === | + | ==== Running the System |
- Open the **CN0202.exe** application from the default installation location. | - Open the **CN0202.exe** application from the default installation location. | ||
- Set the correct connector and SCLK settings for the board in the System Configuration section. | - Set the correct connector and SCLK settings for the board in the System Configuration section. | ||
Line 98: | Line 120: | ||
* [[ADI> | * [[ADI> | ||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |