This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0202 [01 Aug 2017 03:54] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0202 [30 Jul 2021 07:19] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0202 Evaluation Board Guide ====== | ====== CN0202 Evaluation Board Guide ====== | ||
===== Overview ===== | ===== Overview ===== | ||
- | [[ADI>CN202]] a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, | + | [[ADI>CN0202]] is a full function, flexible, programmable analog output solution that meets most requirements for programmable logic controller (PLC) and distributed control system (DCS) applications. It provides all the typical voltage and current output ranges with 16-bit resolution and no missing codes, 0.05% linearity, and less than 0.2% total output error. The circuit also contains key features for industrial applications, |
- | The [[ADI> | + | The [[ADI> |
The [[ADI> | The [[ADI> | ||
Line 14: | Line 14: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Triple Output DC Power Supply (6 V, +15 V and -15 V) | * Triple Output DC Power Supply (6 V, +15 V and -15 V) | ||
+ | * //Agilent E3631A 0 V to 6 V/5 A; ±25 V/1 A Triple Output DC Power Supply// | ||
+ | * Digital Multimeter for Verification (**Optional**) | ||
+ | * //Agilent 34401A 6.5 Digital Multimeter// | ||
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
- | * Windows | + | * Windows |
* USB interface | * USB interface | ||
- | * USB type A to USB type mini-B cable | ||
---- | ---- | ||
===== General Setup ===== | ===== General Setup ===== | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
- | {{ : | + | {{ : |
- | * The [[http:// | + | * The [[adi>EVAL-CN0202-SDPZ|EVAL-CN0202-SDPZ]] **(CN-0202 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * Terminal block CN1 is the +/- 15 V power supply input | + | * Terminal block **CN1** is the +/- 15 V power supply input |
- | * Terminal block CN2 is the +6 V power supply input | + | * Terminal block **CN2** is the +6 V power supply input |
- | * Terminal block CN3 is for the voltage output measurement | + | * Terminal block **CN3** is for the voltage output measurement |
- | * Terminal block CN4 is for the current output measurement | + | * **Optionally**, |
+ | * Terminal block **CN4** is for the current output measurement | ||
\\ | \\ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Do not connect the USB cable to the mini USB connector | + | |
</ | </ | ||
==== Jumper settings ==== | ==== Jumper settings ==== | ||
- | {{ : | + | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> |
+ | |||
+ | {{ : | ||
---- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
- | - Extract the file **CN0202_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | + | - Extract the file **CN0202_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> |
- Click **Next** to view the installation review page\\ \\ {{: | - Click **Next** to view the installation review page\\ \\ {{: | ||
- | - Click **Next** to start the installation\\ \\ {{: | + | - Click **Next** to start the installation\\ \\ {{: |
- Upon completion of the installation of the **CN-0202 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | - Upon completion of the installation of the **CN-0202 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | ||
- | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | + | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: |
- Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
+ | ====Main Tab==== | ||
+ | {{ : | ||
+ | * **Connection** <fc # | ||
+ | * **Connect Button** | ||
+ | * Starts the connection with the [[ADI> | ||
+ | * **Disconnect Button** | ||
+ | * Ends the connection with the [[ADI> | ||
+ | |||
+ | * **System Configuration** <fc # | ||
+ | * **Connector** | ||
+ | * Selects which 120-pin connection of the SDP-B Board to use | ||
+ | * **SLCK** | ||
+ | * Sets the SPI clock frequency used by the evaluation board | ||
+ | |||
+ | * **AD5750-1 Configuration** <fc # | ||
+ | * **JP1 Configuration** | ||
+ | * Sets the SPI address of the AD5750-1 based on the position of JP1 | ||
+ | * **Range Select** | ||
+ | * Sets the voltage/ | ||
+ | * **Toggle CLEAR** | ||
+ | * Sets the outputs to the zero/ | ||
+ | |||
+ | * **AD5750-1 Error Indicator** <fc # | ||
+ | * **Vout Fault** | ||
+ | * There is a short circuit on the VOUT pin | ||
+ | * **Iout Fault** | ||
+ | * There is an open circuit on the IOUT pin | ||
+ | * **Over Temp** | ||
+ | * The AD5750-1 core temperature exceeds 150 °C | ||
+ | * **PEC Error** | ||
+ | * CRC-8 error checking detected an interface error | ||
+ | |||
+ | * **Output Setting** <fc # | ||
+ | * **Write AD5660-1** | ||
+ | * Writes the hexadecimal value in the left field to the AD5660-1 output voltage | ||
+ | * **Reset AD5750-1** | ||
+ | * Resets the AD5750-1 to its power-on state | ||
+ | |||
+ | * **Quit** | ||
+ | * Exits the software application | ||
+ | |||
+ | \\ | ||
+ | ==== Running the System ==== | ||
+ | - Open the **CN0202.exe** application from the default installation location. | ||
+ | - Set the correct connector and SCLK settings for the board in the System Configuration section. | ||
+ | - Click the **Connect Button** | ||
+ | - Upon successful connection, select the desired range of output on the Range Select drop-down menu. | ||
+ | - Input a hex value equivalent of the desired output level in the Output Setting section. | ||
+ | - Click **Write AD5662** | ||
+ | - Click **Disconnect Button** if finished. | ||
+ | |||
+ | |||
---- | ---- | ||
+ | |||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
* [[ftp:// | * [[ftp:// | ||
Line 61: | Line 120: | ||
* [[ADI> | * [[ADI> | ||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |