This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0202 [17 Jul 2017 04:12] – Page Created JB Chua | resources:eval:user-guides:circuits-from-the-lab:cn0202 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | CN0202 Evaluation Board Guide | + | ====== |
+ | ===== Overview ===== | ||
+ | [[ADI> | ||
+ | |||
+ | The [[ADI> | ||
+ | |||
+ | The [[ADI> | ||
+ | The [[ADI> | ||
+ | |||
+ | The EVAL-CN0202-SDPZ board connects to ADI’s System Demonstration Platform (SDP) and is powered by a triple output DC power supply of +15 V, -15 V and 6 V. | ||
+ | {{ : | ||
+ | \\ | ||
+ | ---- | ||
+ | ===== Required Equipment ===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[ftp:// | ||
+ | * Triple Output DC Power Supply (6 V, +15 V and -15 V) | ||
+ | * //Agilent E3631A 0 V to 6 V/5 A; ±25 V/1 A Triple Output DC Power Supply// | ||
+ | * Digital Multimeter for Verification (**Optional**) | ||
+ | * //Agilent 34401A 6.5 Digital Multimeter// | ||
+ | * PC with the following //Minimum Requirements// | ||
+ | * Windows 7 or higher | ||
+ | * USB interface | ||
+ | |||
+ | ---- | ||
+ | ===== General Setup ===== | ||
+ | ==== Block assignments ==== | ||
+ | {{ : | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | * Terminal block **CN1** is the +/- 15 V power supply input | ||
+ | * Terminal block **CN2** is the +6 V power supply input | ||
+ | * Terminal block **CN3** is for the voltage output measurement | ||
+ | * **Optionally**, | ||
+ | * Terminal block **CN4** is for the current output measurement | ||
+ | |||
+ | \\ | ||
+ | |||
+ | <WRAP center round important 60%> | ||
+ | Power on the **(EVAL-CN0202-SDPZ)** through the triple output power supply and the **(SDP-B Board)** through the PC **separately** before connecting the two boards together. | ||
+ | </ | ||
+ | |||
+ | ==== Jumper settings ==== | ||
+ | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ---- | ||
+ | ===== Installing the Evaluation Software ===== | ||
+ | - Extract the file **CN0202_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ \\ {{: | ||
+ | - Click **Next** to start the installation\\ \\ {{: | ||
+ | - Upon completion of the installation of the **CN-0202 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
+ | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
+ | |||
+ | ---- | ||
+ | ===== Using the Evaluation Software ===== | ||
+ | ====Main Tab==== | ||
+ | {{ : | ||
+ | * **Connection** <fc # | ||
+ | * **Connect Button** | ||
+ | * Starts the connection with the [[ADI> | ||
+ | * **Disconnect Button** | ||
+ | * Ends the connection with the [[ADI> | ||
+ | |||
+ | * **System Configuration** <fc # | ||
+ | * **Connector** | ||
+ | * Selects which 120-pin connection of the SDP-B Board to use | ||
+ | * **SLCK** | ||
+ | * Sets the SPI clock frequency used by the evaluation board | ||
+ | |||
+ | * **AD5750-1 Configuration** <fc # | ||
+ | * **JP1 Configuration** | ||
+ | * Sets the SPI address of the AD5750-1 based on the position of JP1 | ||
+ | * **Range Select** | ||
+ | * Sets the voltage/ | ||
+ | * **Toggle CLEAR** | ||
+ | * Sets the outputs to the zero/ | ||
+ | |||
+ | * **AD5750-1 Error Indicator** <fc # | ||
+ | * **Vout Fault** | ||
+ | * There is a short circuit on the VOUT pin | ||
+ | * **Iout Fault** | ||
+ | * There is an open circuit on the IOUT pin | ||
+ | * **Over Temp** | ||
+ | * The AD5750-1 core temperature exceeds 150 °C | ||
+ | * **PEC Error** | ||
+ | * CRC-8 error checking detected an interface error | ||
+ | |||
+ | * **Output Setting** <fc # | ||
+ | * **Write AD5660-1** | ||
+ | * Writes the hexadecimal value in the left field to the AD5660-1 output voltage | ||
+ | * **Reset AD5750-1** | ||
+ | * Resets the AD5750-1 to its power-on state | ||
+ | |||
+ | * **Quit** | ||
+ | * Exits the software application | ||
+ | |||
+ | \\ | ||
+ | ==== Running the System ==== | ||
+ | - Open the **CN0202.exe** application from the default installation location. | ||
+ | - Set the correct connector and SCLK settings for the board in the System Configuration section. | ||
+ | - Click the **Connect Button** | ||
+ | - Upon successful connection, select the desired range of output on the Range Select drop-down menu. | ||
+ | - Input a hex value equivalent of the desired output level in the Output Setting section. | ||
+ | - Click **Write AD5662** | ||
+ | - Click **Disconnect Button** if finished. | ||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== More Information and Useful Links ===== | ||
+ | * [[ftp:// | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ |