This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0198 [30 Jan 2013 22:22] – [Programming Sequence and How to Change the Output After Setting it to a Value] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0198 [30 Jul 2021 07:19] – Victor Calinao, Jr | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * [[http:// | + | * [[adi>AD5755|AD5755]] Evaluation board. |
- | * [[http:// | + | * [[adi>ADP2300|ADP2300]] Evaluation board. |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation board |
* [[ftp:// | * [[ftp:// | ||
* Power Supply: +/-15V supply. | * Power Supply: +/-15V supply. | ||
Line 39: | Line 39: | ||
- Solder one end of a red wire to J3 of the ADP2300 and connect the other end to J6 - pin 1(AVCC) of the AD5755 Evaluation Board. | - Solder one end of a red wire to J3 of the ADP2300 and connect the other end to J6 - pin 1(AVCC) of the AD5755 Evaluation Board. | ||
- {{ : | - {{ : | ||
- | - Using a blue wire, connect J5 pin 1 of the [[http:// | + | - Using a blue wire, connect J5 pin 1 of the [[adi>AD5755|AD5755 Evaluation Board]] to -15V connection of a DC power supply. |
- | - Using a black wire, connect J5 pin 2 of the [[http:// | + | - Using a black wire, connect J5 pin 2 of the [[adi>AD5755|AD5755 Evaluation Board]] to the GND connection of a DC power supply. |
- | - Using a red wire, connect J5 pin 3 of the [[http:// | + | - Using a red wire, connect J5 pin 3 of the [[adi>AD5755|AD5755 Evaluation Board]] to +15V connection of a DC power supply. |
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-SDP-CB1Z| EVAL-SDP-CB1Z]] Evaluation board to connector J9 of the [[adi>AD5755|AD5755 Evaluation Board]]. |
- | - Plug the mini end of the USB cable into connector J1 of the [[http:// | + | - Plug the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z| EVAL-SDP-CB1Z]] Evaluation board. |
- {{ : | - {{ : | ||
Line 54: | Line 54: | ||
- LK1 allows the user to input an off board reference voltage using terminal block J7 as an input. | - LK1 allows the user to input an off board reference voltage using terminal block J7 as an input. | ||
- The reference input must fall between 4.95V and 5.05V to achieve performance specified in the datasheet. | - The reference input must fall between 4.95V and 5.05V to achieve performance specified in the datasheet. | ||
- | - LK2 utilizes an on board +5V reference, the [[http:// | + | - LK2 utilizes an on board +5V reference, the [[adi>ADR02|ADR02]]. |
- | - LK3 provides power to the [[http:// | + | - LK3 provides power to the [[adi>ADR02|ADR02]]. |
{{ : | {{ : | ||
Line 118: | Line 118: | ||
- In the **DAC Control Register** section, click **Write**. | - In the **DAC Control Register** section, click **Write**. | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
- | + | // End of document // |