Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:07]
glai
resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 May 2018 19:16] (current)
Brandon fixed some pictures
Line 36: Line 36:
 ===== Connectors and Jumper Configurations ===== ===== Connectors and Jumper Configurations =====
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​hardware.png|}}+{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​new.png|}}
  
 ==== Description ==== ==== Description ====
Line 68: Line 68:
   * Follow the on screen prompts to install the software   * Follow the on screen prompts to install the software
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​1.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install2.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​3.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install3.png?400|}} \\ 
 +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install4.png?400|}} \\
  
 ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== ===== Downloading Firmware to EVAL-ADuC7061-MKZ =====
-  * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. ​+  * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. ​
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}}
   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​
Line 95: Line 96:
   * **STOP APP**: Closing the CN0196 Evaluation Software   * **STOP APP**: Closing the CN0196 Evaluation Software
 2. Provides control to the following: 2. Provides control to the following:
-  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms <​note>​Pulse width should be less than half of the     Pulse Interval </​note>​+  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms ​ 
 +<​note>​Pulse width should be less than half of the     Pulse Interval</​note>​
   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width
   * **Start/​Stop**:​ Provides continuous and discontinues pulses   * **Start/​Stop**:​ Provides continuous and discontinues pulses
Line 118: Line 120:
 </​WRAP>​ </​WRAP>​
  
 +// End of Document //
   ​   ​
  
resources/eval/user-guides/circuits-from-the-lab/cn0196.1512630431.txt.gz · Last modified: 07 Dec 2017 08:07 by glai