Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 08:01]
glai
resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 May 2018 19:16] (current)
Brandon fixed some pictures
Line 36: Line 36:
 ===== Connectors and Jumper Configurations ===== ===== Connectors and Jumper Configurations =====
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​hardware.png|}}+{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​new.png|}}
  
 ==== Description ==== ==== Description ====
-1. Switch S1: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\  +1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\  
-2. Jumper Link LK1: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V.   \\  +2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V.   \\  
-3. Header J1: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table+3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table
 ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^
 | PWRIN J1-1  | +5V_2  J1-1 | | PWRIN J1-1  | +5V_2  J1-1 |
Line 48: Line 48:
 | PWM0  J2-26 | PWM0_I J1-5 | | PWM0  J2-26 | PWM0_I J1-5 |
 | DVDD  J2-28 | +2V5   J1-3 | | DVDD  J2-28 | +2V5   J1-3 |
-4. Jumper Link LK2: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\  +4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\  
-5. Jumper Link LK3: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\  +5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\  
-6. Connector J3: See below table+6.** Connector J3**: See below table
 ^Pin Number^Description^ ^Pin Number^Description^
 | J3-1  | VDD: Power Supply of the load        | | J3-1  | VDD: Power Supply of the load        |
Line 59: Line 59:
 | J3-6  | GND: Ground connection ​              | | J3-6  | GND: Ground connection ​              |
  
-7. Connector J4: Connects +12V power supply and Ground return ​  \\  +7. **Connector J4**: Connects +12V power supply and Ground return ​  \\  
-8. Connector J2: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\  +8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\  
-9. Jumper link LK4: Shorting this pin sets the VDD voltage to +12V +9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V 
  
 ===== Software and Driver Installation ===== ===== Software and Driver Installation =====
Line 68: Line 68:
   * Follow the on screen prompts to install the software   * Follow the on screen prompts to install the software
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​1.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install2.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​3.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install3.png?400|}} \\ 
 +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install4.png?400|}} \\
  
 ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== ===== Downloading Firmware to EVAL-ADuC7061-MKZ =====
-  * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. ​+  * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. ​
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}}
   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​
Line 95: Line 96:
   * **STOP APP**: Closing the CN0196 Evaluation Software   * **STOP APP**: Closing the CN0196 Evaluation Software
 2. Provides control to the following: 2. Provides control to the following:
-  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms <​note>​Pulse width should be less than half of the     Pulse Interval </​note>​+  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms ​ 
 +<​note>​Pulse width should be less than half of the     Pulse Interval</​note>​
   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width
   * **Start/​Stop**:​ Provides continuous and discontinues pulses   * **Start/​Stop**:​ Provides continuous and discontinues pulses
Line 106: Line 108:
   * **VDD**: Controls the supply voltage up to 20V   * **VDD**: Controls the supply voltage up to 20V
   * **Inductor**:​ Controls the inductor value up to 100mH to be used as a load   * **Inductor**:​ Controls the inductor value up to 100mH to be used as a load
-6. Displays the  Inductor (A) vs Time(s) waveform+6. Displays the  Inductor (A) vs Time(s) waveform ​ 
 + 
 +===== Schematic, PCB Layout, Bill of Materials ===== 
 + 
 +<WRAP round 80% download>​ 
 +[[http://​www.analog.com/​CN0196-DesignSupport|EVAL-CN0196-EB1Z Design & Integration Files]] 
 +  * Schematics  
 +  * PCB Layout  
 +  * Bill of Materials  
 +  * PADS project 
 +</​WRAP>​ 
 + 
 +// End of Document //
   ​   ​
  
resources/eval/user-guides/circuits-from-the-lab/cn0196.1512630093.txt.gz · Last modified: 07 Dec 2017 08:01 by glai