Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0196 [07 Dec 2017 03:59]
glai
resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 May 2018 19:16]
Brandon fixed some pictures
Line 24: Line 24:
  
 ===== General Setup =====  ===== General Setup ===== 
-  * Connect the controlling signal from [[ADI>​EVAL-ADuC7061]] and [[ADI>​CN0196]] according to the jumper configuration found in Connectors and Jumper Configurations below+  * Connect the controlling signal from [[ADI>​EVAL-ADuC7061]] and [[ADI>​CN0196]] according to the jumper configuration found in Connectors and Jumper Configurations ​section ​below
   * Connect the jumpers LK1  pin 1 and 2, LK2 pin 2 and 3, LK3 pin 1 and 2 and short LK4 pin    * Connect the jumpers LK1  pin 1 and 2, LK2 pin 2 and 3, LK3 pin 1 and 2 and short LK4 pin 
   * Apply +12V power supply to J4 of CN0196 board   * Apply +12V power supply to J4 of CN0196 board
Line 36: Line 36:
 ===== Connectors and Jumper Configurations ===== ===== Connectors and Jumper Configurations =====
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​hardware.png|}}+{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​new.png|}}
  
 ==== Description ==== ==== Description ====
- +1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\  
-1. Switch S1: ON state disables ​the isolator inputs and refresh circuits ​\\  +2. **Jumper Link LK1**Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V.   \\  
-2. Jumper Link LK1: \\  +3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table
-3. Header J1: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table+
 ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^
 | PWRIN J1-1  | +5V_2  J1-1 | | PWRIN J1-1  | +5V_2  J1-1 |
Line 49: Line 48:
 | PWM0  J2-26 | PWM0_I J1-5 | | PWM0  J2-26 | PWM0_I J1-5 |
 | DVDD  J2-28 | +2V5   J1-3 | | DVDD  J2-28 | +2V5   J1-3 |
-4. Jumper Link LK2: \\  +4. **Jumper Link LK2**Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\  
-5. Jumper Link LK3: \\  +5. **Jumper Link LK3**If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. ​\\  
-6. Connector J3:  ​\\  +6.** Connector J3**See below table 
-7. Connector J4: Connects +12V power supply and Ground return ​  \\  +^Pin Number^Description^ 
-8. Connector J2: Connection of an external supply up to +20V if jumper link LK4 is not shorted ​+| J3-1  | VDD: Power Supply of the load        | 
 +| J3-2  | VDD: Power Supply of the load        | 
 +| J3-3  | OUT1: Connection of the inductor load| 
 +| J3-4  | OUT2: Connection of the inductor load| 
 +| J3-5  | GND: Ground connection ​              | 
 +| J3-6  | GND: Ground connection ​              | 
 + 
 +7. **Connector J4**: Connects +12V power supply and Ground return ​  \\  
 +8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted ​\\  
 +9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V 
  
 ===== Software and Driver Installation ===== ===== Software and Driver Installation =====
Line 60: Line 68:
   * Follow the on screen prompts to install the software   * Follow the on screen prompts to install the software
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​1.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install2.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​3.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install3.png?400|}} \\ 
 +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install4.png?400|}} \\
  
 ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== ===== Downloading Firmware to EVAL-ADuC7061-MKZ =====
-  * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. ​+  * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. ​
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}}
   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​
Line 85: Line 94:
   * **Connect**:​ Setting up connection between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ   * **Connect**:​ Setting up connection between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ
   * **Disconnect**:​ Disconnects the hardware ​   * **Disconnect**:​ Disconnects the hardware ​
-  * **STOP APP**: Closing the CN0196 Evaluation ​SOftware+  * **STOP APP**: Closing the CN0196 Evaluation ​Software
 2. Provides control to the following: 2. Provides control to the following:
-  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8mz \\ <​note>​Pulse width should be less than half of the pulse interval</​note>​+  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms  
 +<​note>​Pulse width should be less than half of the     Pulse Interval</​note>​
   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width   * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width
   * **Start/​Stop**:​ Provides continuous and discontinues pulses   * **Start/​Stop**:​ Provides continuous and discontinues pulses
Line 96: Line 106:
 4. Displays the current status/​activity being done in the software \\ 4. Displays the current status/​activity being done in the software \\
 5. Provides control to the following: 5. Provides control to the following:
-  * **VDD**: Controls the supply voltage up to 48V+  * **VDD**: Controls the supply voltage up to 20V
   * **Inductor**:​ Controls the inductor value up to 100mH to be used as a load   * **Inductor**:​ Controls the inductor value up to 100mH to be used as a load
-6. Displays the  Inductor (A) vs Time(s) waveform+6. Displays the  Inductor (A) vs Time(s) waveform ​ 
 + 
 +===== Schematic, PCB Layout, Bill of Materials ===== 
 + 
 +<WRAP round 80% download>​ 
 +[[http://​www.analog.com/​CN0196-DesignSupport|EVAL-CN0196-EB1Z Design & Integration Files]] 
 +  * Schematics  
 +  * PCB Layout  
 +  * Bill of Materials  
 +  * PADS project 
 +</​WRAP>​ 
 + 
 +// End of Document //
   ​   ​
  
resources/eval/user-guides/circuits-from-the-lab/cn0196.txt · Last modified: 29 May 2018 19:16 by Brandon