Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0196 [06 Dec 2017 10:03]
glai
resources:eval:user-guides:circuits-from-the-lab:cn0196 [29 May 2018 19:16]
Brandon fixed some pictures
Line 24: Line 24:
  
 ===== General Setup =====  ===== General Setup ===== 
-  * Connect [[ADI>CN0196]] board  to [[ADI>EVAL-ADuC7061]] board according to the table below \\ +  * Connect ​the controlling signal from [[ADI>EVAL-ADuC7061]] and [[ADI>CN0196]] according to the jumper configuration found in Connectors and Jumper Configurations section ​below 
- +  ​* Connect the jumpers LK1  pin and 2, LK2 pin 2 and 3, LK3 pin 1 and and short LK4 pin  
-^ EVAL-ADuC7061MKZ ^ EVAL-CN0196-EB1Z +  ​* Apply +12V power supply to J4 of CN0196 board 
-| PWRIN J1-1  | +5V_2 J1- | +  * Connect the USB cable from PC to the USB mini connector on the EVAL-ADuC7061-MKZ board 
-| GND   J1- | GND2   J1-| +  ​* Connect an inductor as a load between OUT1 and OUT2 of J3
-| PWM1  J2-25 | PWM1_I J1-4 | +
-| PWM0  J2-26 | PWM0_I J1-5 |+
  
 ===== Test Setup Functional Block Diagram =====  ===== Test Setup Functional Block Diagram ===== 
Line 38: Line 36:
 ===== Connectors and Jumper Configurations ===== ===== Connectors and Jumper Configurations =====
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​hardware.png|}}+{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​new.png|}}
  
-**Description**+==== Description ==== 
 +1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\  
 +2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V.   \\  
 +3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table 
 +^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ 
 +| PWRIN J1-1  | +5V_2  J1-1 | 
 +| GND   ​J1-2 ​ | GND2   J1-2 | 
 +| PWM1  J2-25 | PWM1_I J1-4 | 
 +| PWM0  J2-26 | PWM0_I J1-5 | 
 +| DVDD  J2-28 | +2V5   J1-3 | 
 +4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\  
 +5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\  
 +6.** Connector J3**: See below table 
 +^Pin Number^Description^ 
 +| J3-1  | VDD: Power Supply of the load        | 
 +| J3-2  | VDD: Power Supply of the load        | 
 +| J3-3  | OUT1: Connection of the inductor load| 
 +| J3-4  | OUT2: Connection of the inductor load| 
 +| J3-5  | GND: Ground connection ​              | 
 +| J3-6  | GND: Ground connection ​              |
  
-  ​- Switch S1:  +7. **Connector J4**: Connects +12V power supply and Ground return ​  ​\\  
-  - Jumper Link LK1+8. **Connector J2**Connection of an external supply up to +20V if jumper link LK4 is not shorted \\  
-  - Header J1: +9. **Jumper ​link LK4**Shorting this pin sets the VDD voltage to +12V 
-  - Jumper ​Link LK2: +
-  - Jumper Link LK3: +
-  - Connector J3: +
-  - Connector J4 +
-  - Connector J2:+
  
 ===== Software and Driver Installation ===== ===== Software and Driver Installation =====
Line 56: Line 68:
   * Follow the on screen prompts to install the software   * Follow the on screen prompts to install the software
  
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​1.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.1.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install1.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​2.png|}} \\  +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install2.png?400|}} \\ 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​3.png|}} \\ +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install3.png?400|}} \\ 
 +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0393install4.png?400|}} \\
  
 ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== ===== Downloading Firmware to EVAL-ADuC7061-MKZ =====
-  * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. ​+  * Connect the EVAL-ADuC7061-MKZ to the PC using USB cable, then find the COM port assigned to this board in the Device Manager. ​
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​port.png|}}
   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​   * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. ​
Line 74: Line 87:
  
 ===== Using Evaluation Software ===== ===== Using Evaluation Software =====
-== Software Front Panel == +==== Software Front Panel ==== 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​soft1.png|}} +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​sofft1.png|}} 
-{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​soft2.png|}}+{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​sofft2.png|}} 
 +==== Description ==== 
 +1. Provides control to the following: ​  
 +  * **Connect**:​ Setting up connection between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ 
 +  * **Disconnect**:​ Disconnects the hardware  
 +  * **STOP APP**: Closing the CN0196 Evaluation Software 
 +2. Provides control to the following:​ 
 +  * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms  
 +<​note>​Pulse width should be less than half of the     Pulse Interval</​note>​ 
 +  * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width 
 +  * **Start/​Stop**:​ Provides continuous and discontinues pulses 
 +  * **High Side Shot**: When this button is pressed, the PWM waveform will display the Voltage on the high side Mosfets Q1 and Q2  
 +  * **Low Side Shot**: ​ When this button is pressed, the PWM waveform will display the Voltage on the low side Mosfets Q3 and Q4  
 +  * **Reset**: Resets all the configuration and hardware connection 
 +3. Displays the PWM waveform (V) vs Time(s) depending on the configuration set on the PWM controls ​ \\ 
 +4. Displays the current status/​activity being done in the software \\ 
 +5. Provides control to the following:​ 
 +  * **VDD**: Controls the supply voltage up to 20V 
 +  * **Inductor**:​ Controls the inductor value up to 100mH to be used as a load 
 +6. Displays the  Inductor (A) vs Time(s) waveform  
 + 
 +===== Schematic, PCB Layout, Bill of Materials ===== 
 + 
 +<WRAP round 80% download>​ 
 +[[http://​www.analog.com/​CN0196-DesignSupport|EVAL-CN0196-EB1Z Design & Integration Files]] 
 +  * Schematics  
 +  * PCB Layout  
 +  * Bill of Materials  
 +  * PADS project 
 +</​WRAP>​ 
 + 
 +// End of Document // 
 +   
  
-==== Descriptions:​ ==== 
  
-  - Connect: Provides connection between EVAL-CN0196-EB1Z and EVAL-ADuC7061-MKZ boards. 
-  - Disconnect: Provides disconnection between EVAL-CN0196-EB1Z and EVAL-ADuC7061-MKZ boards. 
-  - Stop APP: Stop gathering data 
-  - Load Configuration:​ 
-  - VDD: 
-  - Inductor: 
-  - Enable: 
-  - Maximum Current: 
-  - PWM Waveform: 
-  - PWM Configuration:​ 
-  - PWM Pulse Width: 
-  - PWM Interval: 
-  - Stop: 
-  - High Side Shot: 
-  - Low Side Shot: 
-  - Reset: 
-  - Current Wave:  
  
  
  
  
resources/eval/user-guides/circuits-from-the-lab/cn0196.txt · Last modified: 29 May 2018 19:16 by Brandon