This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0196 [21 Sep 2017 04:27] – Glaizel Arinuelo | resources:eval:user-guides:circuits-from-the-lab:cn0196 [15 Dec 2017 22:57] – Brandon Bushey | ||
---|---|---|---|
Line 14: | Line 14: | ||
{{: | {{: | ||
- | ====== Equipment Needed | + | ===== Equipment Needed ===== |
* PC with a USB port and Windows XP, Windows Vista (32-bit), or Windows 7 (32-bit) | * PC with a USB port and Windows XP, Windows Vista (32-bit), or Windows 7 (32-bit) | ||
Line 22: | Line 22: | ||
* Load, such as Coilcraft SER2014-402 power inductor | * Load, such as Coilcraft SER2014-402 power inductor | ||
* Oscilloscope with current probe | * Oscilloscope with current probe | ||
+ | |||
+ | ===== General Setup ===== | ||
+ | * Connect the controlling signal from [[ADI> | ||
+ | * Connect the jumpers LK1 pin 1 and 2, LK2 pin 2 and 3, LK3 pin 1 and 2 and short LK4 pin | ||
+ | * Apply +12V power supply to J4 of CN0196 board | ||
+ | * Connect the USB cable from PC to the USB mini connector on the EVAL-ADuC7061-MKZ board | ||
+ | * Connect an inductor as a load between OUT1 and OUT2 of J3 | ||
===== Test Setup Functional Block Diagram ===== | ===== Test Setup Functional Block Diagram ===== | ||
{{: | {{: | ||
+ | |||
+ | ===== Connectors and Jumper Configurations ===== | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== Description ==== | ||
+ | 1. **Switch S1**: ON state provides an isolated side PWM pulses, OFF states makes the PWM disappears\\ | ||
+ | 2. **Jumper Link LK1**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. | ||
+ | 3. **Header J1**: Provides connection of the controlling signals between EVAL-CN0196-EB1Z and EVAL-ADuC7061MKZ as seen in below table | ||
+ | ^EVAL-ADuC7061MKZ^EVAL-CN0196-EB1Z^ | ||
+ | | PWRIN J1-1 | +5V_2 J1-1 | | ||
+ | | GND | ||
+ | | PWM1 J2-25 | PWM1_I J1-4 | | ||
+ | | PWM0 J2-26 | PWM0_I J1-5 | | ||
+ | | DVDD J2-28 | +2V5 J1-3 | | ||
+ | 4. **Jumper Link LK2**: Shorting pin 1 and 2 sets the Source Terminal of ADG787 to 5V while pin 2 and 3 sets to 0V. \\ | ||
+ | 5. **Jumper Link LK3**: If pin 1 and 2 is shorted, disabling the ADUM7234 for under voltage condition is generated on board. Shorting pin 2 and 3 will provide externally disabling the isolator via J1-6 header. \\ | ||
+ | 6.** Connector J3**: See below table | ||
+ | ^Pin Number^Description^ | ||
+ | | J3-1 | VDD: Power Supply of the load | | ||
+ | | J3-2 | VDD: Power Supply of the load | | ||
+ | | J3-3 | OUT1: Connection of the inductor load| | ||
+ | | J3-4 | OUT2: Connection of the inductor load| | ||
+ | | J3-5 | GND: Ground connection | ||
+ | | J3-6 | GND: Ground connection | ||
+ | |||
+ | 7. **Connector J4**: Connects +12V power supply and Ground return | ||
+ | 8. **Connector J2**: Connection of an external supply up to +20V if jumper link LK4 is not shorted \\ | ||
+ | 9. **Jumper link LK4**: Shorting this pin sets the VDD voltage to +12V | ||
+ | |||
+ | ===== Software and Driver Installation ===== | ||
+ | * Extract the file [[ftp:// | ||
+ | < | ||
+ | * Follow the on screen prompts to install the software | ||
+ | |||
+ | {{: | ||
+ | {{: | ||
+ | {{: | ||
+ | {{: | ||
+ | |||
+ | ===== Downloading Firmware to EVAL-ADuC7061-MKZ ===== | ||
+ | * Connect the EVAL-ADuV7061-MKZ to the PC using USB cable, then find the port assigned to this board in the Device Manager. | ||
+ | {{: | ||
+ | * Open the software ”ARMWSD.exe” located in the ARMWSD folder, or C:\Program Files\Analog Devices\CN0196\ARMWSD\ARMWSD.exe. | ||
+ | {{: | ||
+ | * Click the Configure | ||
+ | {{: | ||
+ | * Change tab to Commands, set the Flash and Run selection according to the image below. | ||
+ | {{: | ||
+ | * After setting the configuration, | ||
+ | {{: | ||
+ | |||
+ | ===== Using Evaluation Software ===== | ||
+ | ==== Software Front Panel ==== | ||
+ | {{: | ||
+ | {{: | ||
+ | ==== Description ==== | ||
+ | 1. Provides control to the following: | ||
+ | * **Connect**: | ||
+ | * **Disconnect**: | ||
+ | * **STOP APP**: Closing the CN0196 Evaluation Software | ||
+ | 2. Provides control to the following: | ||
+ | * **PWM Pulse Width**: Sets the PWM pulse width up to 12.8ms | ||
+ | < | ||
+ | * **PWM Interval**: Sets the PWM interval up to 12.8ms depending on the configured PWM pulse width | ||
+ | * **Start/ | ||
+ | * **High Side Shot**: When this button is pressed, the PWM waveform will display the Voltage on the high side Mosfets Q1 and Q2 | ||
+ | * **Low Side Shot**: | ||
+ | * **Reset**: Resets all the configuration and hardware connection | ||
+ | 3. Displays the PWM waveform (V) vs Time(s) depending on the configuration set on the PWM controls | ||
+ | 4. Displays the current status/ | ||
+ | 5. Provides control to the following: | ||
+ | * **VDD**: Controls the supply voltage up to 20V | ||
+ | * **Inductor**: | ||
+ | 6. Displays the Inductor (A) vs Time(s) waveform | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[http:// | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | // End of Document // | ||
+ | | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||