This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0194 [19 Apr 2018 09:39] – Jesse Daniel Santos | resources:eval:user-guides:circuits-from-the-lab:cn0194 [30 Jul 2021 07:17] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 4: | Line 4: | ||
{{: | {{: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>EVAL-CN0194-SDPZ|EVAL-CN0194-SDPZ]] Evaluation Board (**CN-0194 Board**) |
* Power Supply | * Power Supply | ||
* Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA. | * Adjustable DC power supply, output should satisfy: from +6V to +12V over than 500mA. | ||
Line 22: | Line 22: | ||
* CN0194 SDP Evaluation Software | * CN0194 SDP Evaluation Software | ||
* Supplied with CD | * Supplied with CD | ||
- | ===== General Setup ===== | + | |
- | + | ||
- | | + | |
- | * Use the Adjustable DC power supplies to powers the [[http://www.analog.com/ | + | |
- | * The [[http:// | + | |
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
+ | ==== General Setup ==== | ||
+ | * EVAL-CN0194-SDPZ connects to the SDP-B Board via the 120-Pin connector **CON A** | ||
+ | * Connect +6V DC power supplies on the **J1** and **J2** connectors to power the EVAL-CN0194-SDPZ | ||
+ | * - EVAL-CN0194-SDPZ is ready to use if diodes **D3**, **D4**, and **D7** light up. | ||
+ | * The EVAL-SDP-CB1Z connects to the PC via the USB cable. | ||
+ | * Apply the input signals on the provided points on the board labeled **AIN1** and **AIN2**. | ||
===== Installing the Software ===== | ===== Installing the Software ===== | ||
Line 41: | Line 43: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Software Control and Indicator Descriptions ==== | ==== Software Control and Indicator Descriptions ==== | ||
+ | {{: | ||
-**Connect/ | -**Connect/ | ||
* When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped. | * When this button is clicked, the SDP-B Board USB connection to the CN-0194 Board status will be filliped. | ||
Line 54: | Line 57: | ||
* Sets which channel is used and displayed. | * Sets which channel is used and displayed. | ||
-**Control Tabs** | -**Control Tabs** | ||
- | * __Time Domain__ : This Tab showing | + | * __Time Domain__ : This tab shows the signal received |
- | * __Frequency Domain__ : This Tab include two indicators to showing the position and velocity output of RDC, update in real time when RDC is converting. | + | * __Frequency Domain__ : This tab shows the signal received in the ADC plotted in amplitude vs frequency. |
- | * __Histogram__ : | + | * __Histogram__ : This tab shows distribution of the captured signal amplitude displayed as the ADC code. |
* __S/W Version Info__ : Showing the SDP-B Board information when USB connection available. | * __S/W Version Info__ : Showing the SDP-B Board information when USB connection available. | ||
-**Navigation Tools** | -**Navigation Tools** | ||
- | * __Cursor__ | + | * __Cursor__ |
* __Magnification__ : Contains magnification tools | * __Magnification__ : Contains magnification tools | ||
* __Hand__ : Used for navigating through the graph | * __Hand__ : Used for navigating through the graph | ||
Line 69: | Line 72: | ||
* This indicator displays a message regarding the status of the SDP-B Board. | * This indicator displays a message regarding the status of the SDP-B Board. | ||
-**Status LED** | -**Status LED** | ||
- | * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off. | + | * This LED showing the ADC working status, when ADC is converting this LED will be light up, otherwise it will be turn off. |
-**Frequency Analysis** | -**Frequency Analysis** | ||
* __THD__ : Total harmonic distortion | * __THD__ : Total harmonic distortion | ||
Line 81: | Line 84: | ||
-** SDP Firmware Revision Details ** | -** SDP Firmware Revision Details ** | ||
* __Major Rev__: | * __Major Rev__: | ||
- | * _Minor | + | * __Minor |
* __Date__: | * __Date__: | ||
* __Host Code Rev__: | * __Host Code Rev__: | ||
* __BF Code Rev__: | * __BF Code Rev__: | ||
- | * __Time__: | + | * __Time__: |
- | \\ \\ | + | \\ |
---- | ---- | ||
+ | |||
==== Establishing a USB Connection Link ==== | ==== Establishing a USB Connection Link ==== | ||
- Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | - Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | ||
Line 101: | Line 105: | ||
- When the number of samples reached the samples setting the converting will stop. | - When the number of samples reached the samples setting the converting will stop. | ||
- Click the **Save Data Button** to save the conversion data. | - Click the **Save Data Button** to save the conversion data. | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ |