This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0189 [16 Oct 2012 21:42] – [Step by Step Instruction to Calibrate the Accelerometer] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0189 [30 Jul 2021 07:15] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The [[http:// | + | The [[adi>adxl203|ADXL203]] is a polysilicon surface micromachined sensor and signal conditioning circuit. Acceleration in the X or Y axis will produce a corresponding output voltage on the XOUT or YOUT output pins of the device. The X axis and Y axis are perpendicular to one another.The [[adi>AD8608|AD8608]] quad op amp buffers, attenuates, and level shifts the [[adi>adxl203|ADXL203]] outputs so they are at the proper levels to drive the inputs of the The [[adi>AD7887|AD7887]]. The [[adi>AD7887|AD7887]] is configurable for either dual or single channel operation via the on-chip control register. In this application it is configured for dual channel mode, allowing the user to monitor both outputs of the [[adi>adxl203|ADXL203]], |
===== General Setup ===== | ===== General Setup ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0189-SDPZ|EVAL-CN0189-SDPZ]] Evaluation board. |
* One SDP Controller board: | * One SDP Controller board: | ||
- | * [[http:// | + | * [[adi>SDP-S| EVAL-SDP-CS1Z]] SDP Evaluation board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z| EVAL-SDP-CB1Z]] SDP Evaluation board |
* [[ftp:// | * [[ftp:// | ||
- | * 1 Six Volt DC Wall Wart ([[http:// | + | * 1 Six Volt DC Wall Wart ([[adi>EVAL-CFTL-6V-PWRZ| EVAL-CFTL-6V-PWRZ]]) |
* 1 USB Type-A plug to USB Mini-B plug cable | * 1 USB Type-A plug to USB Mini-B plug cable | ||
- | {{ : | + | {{ : |
===== Minimum PC/System Requirements ===== | ===== Minimum PC/System Requirements ===== | ||
* One PC with the following | * One PC with the following | ||
Line 20: | Line 20: | ||
===== How to Install the Evaluation Software ===== | ===== How to Install the Evaluation Software ===== | ||
- | - Extract the files within the file **CN0189 SDP Eval Software.zip** and open the file **setup.exe**. | + | - Extract the files within the file **CN0189 SDP Eval Software.zip** and open the file **setup.exe**. |
- | - Press **“Next”**.{{ : | + | - Press **“Next”**.{{ : |
- Press **“Next”**. | - Press **“Next”**. | ||
- | - Upon completion of the installation of the **CN0189 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. | + | - Upon completion of the installation of the **CN0189 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. |
- Press **“Next”**. | - Press **“Next”**. | ||
- It is recommended that you install the drivers to the default directory path **C: | - It is recommended that you install the drivers to the default directory path **C: | ||
- Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0189-SDPZ** | - Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0189-SDPZ** | ||
===== Step by Step Instruction for Connecting the Hardware ===== | ===== Step by Step Instruction for Connecting the Hardware ===== | ||
- | - Connect the [[http:// | + | - Connect the [[adi>SDP-S|EVAL-SDP-CS1Z]] and the [[adi>eval-cn0189-sdpz|EVAL-CN0189-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards.{{: |
- | {{: | + | {{: |
- | - Plug in the DC barrel jack to connector J3 of the [[http:// | + | - Plug in the DC barrel jack to connector J3 of the [[adi>eval-cn0189-sdpz|EVAL-CN0189-SDPZ]] and the mini end of the USB cable into connector J2 of the [[adi>SDP-S|EVAL-SDP-CS1Z]]. And connect the other end of the USB cable into the Laptop or PC. |
- | {{: | + | {{: |
- | {{: | + | {{: |
===== Opening and Enabling the Evaluation Software ===== | ===== Opening and Enabling the Evaluation Software ===== | ||
- Launch the executable found at **C: | - Launch the executable found at **C: | ||
- | {{ : | + | {{ : |
===== Step by Step Instruction to Using the Evaluation Software ===== | ===== Step by Step Instruction to Using the Evaluation Software ===== | ||
- The following is a list of all available software controls, grouped according to their location in the software: | - The following is a list of all available software controls, grouped according to their location in the software: | ||
- **System Controls** | - **System Controls** | ||
- | - **Connect** – This button configures the [[http:// | + | - **Connect** – This button configures the [[adi>ad7887|AD7887]] by writing to the necessary registers. |
- | - **Disconnect** – This button will disconnect the [[http:// | + | - **Disconnect** – This button will disconnect the [[adi>eval-cn0189-sdpz|EVAL-CN0189-SDPZ]] board. |
- **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | ||
- **Conversion Mode Controls** - | - **Conversion Mode Controls** - | ||
Line 61: | Line 60: | ||
- Select **Single Sample** in the **Conversion Mode Controls**. | - Select **Single Sample** in the **Conversion Mode Controls**. | ||
- Navigate to the **Calibrate** tab. | - Navigate to the **Calibrate** tab. | ||
- | - To manually enter or change calibration coefficients, | + | - To manually enter or change calibration coefficients, |
- To perform a four point calibration, | - To perform a four point calibration, | ||
- | - Orient the PCB as displayed in the image below.{{ : | + | - Orient the PCB as displayed in the image below.{{ : |
- Press **Sample Data** while rotating the PCB to find the largest output voltage for the X-axis. | - Press **Sample Data** while rotating the PCB to find the largest output voltage for the X-axis. | ||
- | - Orient the PCB as displayed in the image below.{{ : | + | - Orient the PCB as displayed in the image below.{{ : |
- Press **Sample Data** while rotating the PCB to find the smallest output voltage for the X-axis. | - Press **Sample Data** while rotating the PCB to find the smallest output voltage for the X-axis. | ||
- | - Orient the PCB as displayed in the image below.{{ : | + | - Orient the PCB as displayed in the image below.{{ : |
- Press **Sample Data** while rotating the PCB to find the largest output voltage for the Y-axis. | - Press **Sample Data** while rotating the PCB to find the largest output voltage for the Y-axis. | ||
- | - Orient the PCB as displayed in the image below.{{ : | + | - Orient the PCB as displayed in the image below.{{ : |
- Press **Sample Data** while rotating the PCB to find the smallest output voltage for the Y-axis. | - Press **Sample Data** while rotating the PCB to find the smallest output voltage for the Y-axis. | ||
- Press **Calibrate** to calculate the offset and sensitivity values for each axis. | - Press **Calibrate** to calculate the offset and sensitivity values for each axis. | ||
- Now any further calculations or conversions performed anywhere in the software (**Demonstration** tab or **Sampled Data** tab) will utilize the offset and sensitivity values calculated here. | - Now any further calculations or conversions performed anywhere in the software (**Demonstration** tab or **Sampled Data** tab) will utilize the offset and sensitivity values calculated here. | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |