Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0188 [03 Nov 2017 03:52]
Trisha Cabildo update
resources:eval:user-guides:circuits-from-the-lab:cn0188 [30 Jul 2021 07:14] (current)
Victor Calinao, Jr
Line 15: Line 15:
 ===== Required Equipment ===== ===== Required Equipment =====
   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]
-  * [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)+  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * Power Supply   * Power Supply
Line 29: Line 29:
 ==== Block assignments ==== ==== Block assignments ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-20-01_pm.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-20-01_pm.png?​nolink&​600 |}}\\
-  * The [[http://​www.analog.com/​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector +  * The [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector 
-  * The [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.+  * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input
   * Terminal block **J3** is the test point for 6 V DC output   * Terminal block **J3** is the test point for 6 V DC output
Line 39: Line 39:
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-30-58_pm.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-30-58_pm.png?​nolink&​600 |}}\\
  
-  - Connect the 120-pin connector on the [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board+  - Connect the 120-pin connector on the [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board
   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above
   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board
Line 66: Line 66:
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ====Test Setup Tab==== ====Test Setup Tab====
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​7.png?​nolink&​500 |}}\\ +==== Main Window ==== 
-  ​+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​8.png?​nolink&​700 |}} 
 +  - **Connect** Button - Starts the connection between the [[ADI>​CN0188|CN0188 Evaluation Board]] and [[ADI>​EVAL-SDP-CB1Z|SDP-B Controller Board]]. 
 +  - **Disconnect** Button - Ends the connection between the [[ADI>​CN0188|CN0188 Evaluation Board]] and [[ADI>​EVAL-SDP-CB1Z|SDP-B Controller Board]] 
 +  - **Select SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use 
 +  - **Shunt Voltage Input** - Determines input shunt voltage level in millivolts 
 +  - **Temperature** - Temperature level test conditions of input signal 
 +  - **Data Acquisition** Controls ​\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11.png?​nolink&​600 |}} 
 +      * **Sample Data** - Start acquisition of measurement data  
 +      * **Remove Data Point** - Remove a data point from samples 
 +      * **Save Data** - Save measurement data to file 
 +      * **Clear Data** - Clear the current measurement data 
 +  ​- **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​12.png?​nolink&​600 |}} 
 +      * **ADC Code Plot** Enable - Show or hide the ADC Code plot  
 +      * **Error Plot** Enable - Show or hide the Error plot 
 +      * **Converted Shunt Voltage** - Shunt voltage value from the ADC 
 +      * **Over/​Under Voltage** Indicator - Indicates over or under voltage conditions 
 +      * **Plot Options** - Edit plot display and options like interpolation and color of output waveform 
 +  - **Administration** Tab \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​10.png?​nolink&​600 |}} 
 +      * **Flash LED** - Flashes the LED on the SDP controller board 
 +      * **Read Firmware** - Reads the firmware of CN0240 Evaluation Board  
 +  - **Quit** Button - Closes the evaluation software\\ ​
 \\ \\
  
 +==== Running the System ====
 +  -Open the CN0188.exe application from the default installation location
 +  -Set the correct connector and click the Connect Button
 +  -Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature
 +  -Start and control data acquisition through the data acquisition control buttons
 +  -Output data will be shown in the graph. Edit graph through plot options and check boxes provided
 +  -Click Disconnect if finished
 +  -Click Quit to exit the program
 +
 +\\
 ---- ----
  
Line 75: Line 105:
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * [[ADI>​CN0188|CN0188 Circuit Note Page]]   * [[ADI>​CN0188|CN0188 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]
  
   * [[ADI>​AD7171|AD7171 Product Page]]   * [[ADI>​AD7171|AD7171 Product Page]]
Line 85: Line 115:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
Line 91: Line 121:
   * PADS project   * PADS project
 </​WRAP>​ </​WRAP>​
 +
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0188-SDPZ?&​v=Rev C|Register]] to receive all these great benefits and more!</​WRAP>​
  
 //End of Document// //End of Document//
  
resources/eval/user-guides/circuits-from-the-lab/cn0188.1509677532.txt.gz · Last modified: 03 Nov 2017 03:52 by Trisha Cabildo