Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0188 [26 Oct 2017 09:22]
Trisha Cabildo created
resources:eval:user-guides:circuits-from-the-lab:cn0188 [30 Jul 2021 07:14] (current)
Victor Calinao, Jr
Line 15: Line 15:
 ===== Required Equipment ===== ===== Required Equipment =====
   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]
-  * [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)+  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * Power Supply   * Power Supply
Line 28: Line 28:
 ===== General Setup ===== ===== General Setup =====
 ==== Block assignments ==== ==== Block assignments ====
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​cn0188-00-1024.png?​nolink&​650 |}}\\+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-20-01_pm.png?​nolink&​600 |}}\\ 
 +  * The [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector 
 +  * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. 
 +  * Terminal block **J2** is the +6 V barrel connector for wall wart supply input 
 +  * Terminal block **J3** is the test point for 6 V DC output 
 +  * Terminal block **J4** contains the input terminals for Rshunt and load to ground 
 + 
 +\\ 
 +==== Test setup ==== 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0188:11-2-2017_2-30-58_pm.png?​nolink&​600 |}}\\ 
 + 
 +  - Connect the 120-pin connector on the [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board 
 +  - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above 
 +  - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board 
 +      *//If available, a +6 V "wall wart" can be connected to the barrel connector on the board and used in place of the +6 V power supply// 
 +  - Connect the USB cable supplied with the SDP board to the USB port on the PC 
 +  - Apply power to the +6 V supply (or “wall wart”) connected to [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] 
 +  - Launch the evaluation software 
 +  - Connect the USB cable from the PC to the USB mini connector on the SDP board
  
 \\ \\
  
 <WRAP center round important 60%> <WRAP center round important 60%>
- Do **not** connect ​the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the **EVAL-CN0188-SDPZ**.+ Connect the **system ground** and the **PCB isolated ground** ​to guarantee correct voltage levels and operation. ​**Test point 31** and **test point 32** give access to the GND_ISO required to properly make this connection.
 </​WRAP>​ </​WRAP>​
  
Line 48: Line 66:
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ====Test Setup Tab==== ====Test Setup Tab====
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​7.png?​nolink&​500 |}}\\ +==== Main Window ==== 
-  ​+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​8.png?​nolink&​700 |}} 
 +  - **Connect** Button - Starts the connection between the [[ADI>​CN0188|CN0188 Evaluation Board]] and [[ADI>​EVAL-SDP-CB1Z|SDP-B Controller Board]]. 
 +  - **Disconnect** Button - Ends the connection between the [[ADI>​CN0188|CN0188 Evaluation Board]] and [[ADI>​EVAL-SDP-CB1Z|SDP-B Controller Board]] 
 +  - **Select SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use 
 +  - **Shunt Voltage Input** - Determines input shunt voltage level in millivolts 
 +  - **Temperature** - Temperature level test conditions of input signal 
 +  - **Data Acquisition** Controls ​\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11.png?​nolink&​600 |}} 
 +      * **Sample Data** - Start acquisition of measurement data  
 +      * **Remove Data Point** - Remove a data point from samples 
 +      * **Save Data** - Save measurement data to file 
 +      * **Clear Data** - Clear the current measurement data 
 +  ​- **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​12.png?​nolink&​600 |}} 
 +      * **ADC Code Plot** Enable - Show or hide the ADC Code plot  
 +      * **Error Plot** Enable - Show or hide the Error plot 
 +      * **Converted Shunt Voltage** - Shunt voltage value from the ADC 
 +      * **Over/​Under Voltage** Indicator - Indicates over or under voltage conditions 
 +      * **Plot Options** - Edit plot display and options like interpolation and color of output waveform 
 +  - **Administration** Tab \\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​10.png?​nolink&​600 |}} 
 +      * **Flash LED** - Flashes the LED on the SDP controller board 
 +      * **Read Firmware** - Reads the firmware of CN0240 Evaluation Board  
 +  - **Quit** Button - Closes the evaluation software\\ ​
 \\ \\
  
 +==== Running the System ====
 +  -Open the CN0188.exe application from the default installation location
 +  -Set the correct connector and click the Connect Button
 +  -Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature
 +  -Start and control data acquisition through the data acquisition control buttons
 +  -Output data will be shown in the graph. Edit graph through plot options and check boxes provided
 +  -Click Disconnect if finished
 +  -Click Quit to exit the program
 +
 +\\
 ---- ----
  
Line 57: Line 105:
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * [[ADI>​CN0188|CN0188 Circuit Note Page]]   * [[ADI>​CN0188|CN0188 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]
  
   * [[ADI>​AD7171|AD7171 Product Page]]   * [[ADI>​AD7171|AD7171 Product Page]]
Line 67: Line 115:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
Line 73: Line 121:
   * PADS project   * PADS project
 </​WRAP>​ </​WRAP>​
 +
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0188-SDPZ?&​v=Rev C|Register]] to receive all these great benefits and more!</​WRAP>​
  
 //End of Document// //End of Document//
  
resources/eval/user-guides/circuits-from-the-lab/cn0188.1509002554.txt.gz · Last modified: 26 Oct 2017 09:22 by Trisha Cabildo